PN5180 Dynamic Power Adjustment -> Make maximum

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180 Dynamic Power Adjustment -> Make maximum

2,350件の閲覧回数
riley_baird
Contributor I

I am attempting to output maximum power with the NFC reader on the PN5180 board. It currently specifies that it will adjust its power output according to the proximity of the tag (lower power with closer proximity), but I want to maximize it to always output full power, or even more than it does by default.

I used the software to tune according to the distance (I can find that doc if need be), but it didn't mention how to maximize. Could I get some guidance here?

タグ(2)
0 件の賞賛
返信
1 返信

2,289件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi ,

Hope you are doing great, please check the https://www.nxp.com/docs/en/application-note/AN11742.pdf  , section 1.2.1.1  you can find a note where it explains how to set the DPC  to one gear so it works the way you want.

Have a great day !

BR

Jonathan

0 件の賞賛
返信