PDUM_eAPduFreeAPduInstance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDUM_eAPduFreeAPduInstance

1,963件の閲覧回数
854648943
Contributor III

HI,I need your help with some questions

When i use this function ZPS_eAplAfUnicastAckDataReq( ), I need to apply for some APUD.

I know this function  ZPS_eAplAfUnicastAckDataReq have Retransmission mechanism, so I would like to know if releasing the APDU immediately,will affect subsequent retransmissions?

The function ZPS_eAplAfUnicastAckDataReq,Will it release itself if it's sent?

韩

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,875件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

Releasing the APDU shouldn't have an impact in the possible retransmissions. As for the ZPS_eAplAfUnicastAckDataReq function, the APDU is not automatically freed or released, so you should use the FreeAPDU function after the request.

 

Please let me know if you need any other information.

 

Best regards,

Sebastian

1,875件の閲覧回数
854648943
Contributor III

OK,Thank you for your reply

0 件の賞賛
返信