NXP ls1088ardb booting from sd card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP ls1088ardb booting from sd card

1,202 Views
Rusanya_T
Contributor I

NOTICE: UDIMM 18ADF2G72AZ-2G6E1
ERROR: Board parameters no match.
ERROR: Failed matching board timing.
ERROR: Found training error(s): 0x2100
ERROR: Error: Waiting for D_INIT timeout.
ERROR: Writing DDR register(s) failed
ERROR: Programing DDRC error
ERROR: DDR init failed.
NOTICE: Incorrect DRAM0 size is defined in platfor_def.h
ERROR: mmap_add_region_check() failed. error -22
ERROR: mmap_add_region_check() failed. error -22
NOTICE: BL2: v1.5(release):LSDK-20.12
NOTICE: BL2: Built : 04:35:28, Dec 11 2020
this is the output when I try to boot the ls1088ardb board using sd card. how to fix this error

RusanyaT
0 Kudos
Reply
0 Replies