NTAG 424 ACCES RIGHTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG 424 ACCES RIGHTS

3,489件の閲覧回数
kicedric78
Contributor III

Hello, how are you? what are the definitions of the different access rights (0E, 01,02,03,04,0F)

@Jonathan_Iglesias  HI

0 件の賞賛
返信
3 返答(返信)

3,476件の閲覧回数
kicedric78
Contributor III

Thank you, I understand better, but I still cannot read the tag with my phone (tagWritter with samsung s5), the read access key being on 0E, should I do other additional configurations?

0 件の賞賛
返信

3,481件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi kicedric78,

the access rights basically have 3 different meanings:

if  you put 00,01,02,03,04  it means that operation can be done by the key number you select,  for example if you have for read access:04 it means that in order to read that file you need to be authenticated with key 04.

if you put 0E, it means free access, again if you put this for read access, again for example in read access if you put 0E it means you do not need to be authenticated  in order to read the file.

and 0F is the opposite of 0E, 0F means that there is no access.

 

and they key access set are :

Read,Write, Read/Write, change.

this can be found in section 8.2.3.3 of the DS https://www.nxp.com/docs/en/data-sheet/NT4H2421Gx.pdf

BR

 

Jonathan

3,463件の閲覧回数
kicedric78
Contributor III
Note, the tag is not detected by my phone, are there other configurations so that the tag can be read by a phone (TagWritter)? I took care to set the right access to 0E and write an NDEF message (text)
0 件の賞賛
返信