LIN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,339件の閲覧回数
hamid_abrishami
Contributor III

Hi
I want to use LIN protocol in my project I used MC33662LEF in last project but now in new revision of datasheet we have MC33662BLEF I want to now dose we have any major difference between them. 
and can I use use them instead of each other. 
I saw in some site that said MC33662 is "not recommended for new device" but in data sheet doesn't seen about not recommended 
thanks a lot.
BR.

0 件の賞賛
返信
1 解決策
4,330件の閲覧回数
hamid_abrishami
Contributor III

I found that that LEF par number is not recommended for new devices and BLEF and LEF is similar to each other and just have some little difference:

In Sleep mode, the total module current consumption may be higher than expected if the external pull-up resistor on the RxD pin
is implemented. There may be an unexpected glitch on RxD as INH goes low.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,331件の閲覧回数
hamid_abrishami
Contributor III

I found that that LEF par number is not recommended for new devices and BLEF and LEF is similar to each other and just have some little difference:

In Sleep mode, the total module current consumption may be higher than expected if the external pull-up resistor on the RxD pin
is implemented. There may be an unexpected glitch on RxD as INH goes low.

0 件の賞賛
返信