K12 Chip reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K12 Chip reset

3,043 Views
zcm221
Contributor I

MK12DN512 的Reset 管脚电压约1.6V左右,无法达到正常3.3V,外围电路均正确。这是芯片损坏还是什么原因?谢谢

0 Kudos
Reply
4 Replies

2,984 Views
zcm221
Contributor I

您好,谢谢您的回答,电路一切正常,芯片用了好几年了。今天用一新的JLINK(非正版)在一块原来工作正常的板上下载试了一下,情况依旧,原来工作正常的电路板一下完复位脚即变为1.6V,由于最近在家工作,没示波器看波形,也可能是有脉冲波形,万用表量1.6V左右。前几天调试均工作都可以正常进行,突然出现的情况,现在工作只能停顿了。谢谢

0 Kudos
Reply

2,984 Views
kerryzhou
NXP TechSupport
NXP TechSupport

你内核能找到吗?

你是说你已经能够下载代码,而且代码已经下进去,然后引脚是1.6V reset?你电源电压对不对?

还有能不能debug?能的话,看看debug代码,是否和你说的数组有关?

 另外,你的芯片哪里买的?是否正规渠道?

Wish it helps you!

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,984 Views
zcm221
Contributor I

似乎发现了一个问题所在:程序中有4个数组相加有32K多几个字节,将数组总和降到32K以内,则一切正常。MK12DN512有64K内存,不知是不是对数组的限制的原因。谢谢

0 Kudos
Reply

2,984 Views
kerryzhou
NXP TechSupport
NXP TechSupport

楼主你好!

问你几个问题:

1. 你的芯片是否是第一次使用,完全新的芯片,没有烧过任何的代码?

2. 你是否使用示波器去测试reset引脚的波形,是否是锯齿波?

3. 你的reset引脚是否上拉4.7K 到10K的电阻,对地0.1uf电容?

如果上面都确认是对的话,那么你目前芯片是正常的,我不知道你的1.6V是怎么测试的,或许是直接万用表测试直流电压,这样你的引脚如果是锯齿波的话,这样的电压是算正常。

现在再说下新的芯片没有烧过代码,那么reset引脚会一直产生一个锯齿波,等你烧完代码之后,这个引脚电平就会一直为高正常了。

希望能帮到你,如果还有问题,欢迎继续交流!

Wish it helps you!

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply