First steps with NXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

First steps with NXP

2,016 Views
pavlinstoyanoff
Contributor I

Greetings! I am about to work with your mcus for a very first time. I want to use i.mx rt 1020. What is the prefered tool for programming and debugging? Do you have a special tool for manufacture programming?

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,773 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello Pavlin,

Excellent choice! NXP has its own IDE, is called MCUXpresso, it can download it by following this link in the Downloads tab: https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools/mcuxpresso-in... . This IDE is also used for our Kinetis and LPC MCUs, which you can also evaluate them as well.

The i.MX RT has its own Evaluation kit: https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/i.mx-rt1020-eva... . You are very welcome to check the Documentation and Software available that will provide you some guidance for your project. I may also recommend you to download the RT 1020 SDK, which is a bundle of different examples to give you an easier start on your project: https://mcuxpresso.nxp.com/en/select

In the search bar, you just need to write the name of your board and then click on the Build MCUXpresso SDK button. After this, just download and import it into the already installed MCUXpresso IDE.

Best Regards,
Fabian
0 Kudos
Reply