Explore NFC Board support for Raspberry Pi 4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Explore NFC Board support for Raspberry Pi 4

2,230 Views
jakob1524
Contributor I

Hello,

i have a question about the product EXPLORE NFC Board for Raspberry Pi.

Does this board support the usage with the Raspberry Pi 4?

Because I am having some troubles with the linked NFC Reader Library for Linux V4

I am able to start the examples but e.g the Basic Discovery Loop does not return anything if an NFC Tag touches the Reader.

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

2,103 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

So far, just the SPI protocol is supported for the communication between reader IC and the Raspberry Pi, would you please check if the spi port has been set up correctly?

1.sudo raspi-config .
2.Advanced Options →SPI<Yes>
3.sudo reboot .

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply