Explore NFC Board support for Raspberry Pi 4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Explore NFC Board support for Raspberry Pi 4

2,207件の閲覧回数
jakob1524
Contributor I

Hello,

i have a question about the product EXPLORE NFC Board for Raspberry Pi.

Does this board support the usage with the Raspberry Pi 4?

Because I am having some troubles with the linked NFC Reader Library for Linux V4

I am able to start the examples but e.g the Basic Discovery Loop does not return anything if an NFC Tag touches the Reader.

Thank you

ラベル(1)
0 件の賞賛
返信
1 返信

2,080件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

So far, just the SPI protocol is supported for the communication between reader IC and the Raspberry Pi, would you please check if the spi port has been set up correctly?

1.sudo raspi-config .
2.Advanced Options →SPI<Yes>
3.sudo reboot .

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信