ANTENNA DESIGN FOR HTRC11001T

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ANTENNA DESIGN FOR HTRC11001T

2,882件の閲覧回数
manoj_chate
Contributor I

Hello ,

I want to use HTRC11001T/02EE,11  as my RFID reader option for 125KHz. Since there's no evaluation kit available nor any reference design based on this , I'm unable to define the antenna for this chip. Is there any support or eval kit which defines antenna details for 125 KHz operation ?

Thanks

ラベル(4)
0 件の賞賛
返信
1 返信

2,690件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

Please kindly refer to https://www.nxp.com/docs/en/application-note/AN98080.pdf  for details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信