2 Questions about FlexRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2 Questions about FlexRAM

Jump to solution
7,435 Views
kmh48301
Contributor IV

Hi. I'm using S32k144.

But the forum dosen't work for me. so I'm posting here.

 

1. FlexRAM is slower than SRAM

 

Please see the attachment. (it's from AN11983 p11)

 

When I see flash memory map, I think FlexRAM is also contiguous addresses.

but this is saying non-contiguous...

and is that why the FlexRAM is slower than SRAM?

FlexRAM is not static RAM (SRAM)?

 

2. "a background pattern of all ones" ???

I saw "a background pattern of all ones" several times in NXP documents..

But I have no idea what it means since I'm not native English speaker,,

 

 

Please explain to me

 

Thanks

Best regards,

Phillip

Labels (1)
0 Kudos
Reply
1 Solution
7,405 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

1. This is given by architecture, not by the RAM itself. As you can see, the memories are sitting on different places which inserts some difference:

lukaszadrapa_0-1599466625438.pnglukaszadrapa_0-1599466625438.png

2. "background pattern of all ones"  means, that memory controller will initialize all bytes in FlexRAM allocated for EEE to "0xFF" (all ones) and then it will copy down valid data/records from backup flash. So, non-written words have default value 0xFFFFFFFF.

Regards,

Lukas

 

 

View solution in original post

3 Replies
7,392 Views
kmh48301
Contributor IV

Thank you so much. i thought wrong way. hahaha

0 Kudos
Reply
7,432 Views
kmh48301
Contributor IV

1.

kmh48301_1-1599099331237.pngkmh48301_1-1599099331237.png

 

2.

kmh48301_0-1599099302719.pngkmh48301_0-1599099302719.png

 

0 Kudos
Reply
7,406 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

1. This is given by architecture, not by the RAM itself. As you can see, the memories are sitting on different places which inserts some difference:

lukaszadrapa_0-1599466625438.pnglukaszadrapa_0-1599466625438.png

2. "background pattern of all ones"  means, that memory controller will initialize all bytes in FlexRAM allocated for EEE to "0xFF" (all ones) and then it will copy down valid data/records from backup flash. So, non-written words have default value 0xFFFFFFFF.

Regards,

Lukas