NXP Designs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Designs Knowledge Base

Discussions

Sort by:
本文说明在S32G上如何只用QSPI Nor启动一个最小Linux,最主要的作用是:Linux的紧急/升级/测试模式,或快速启动 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 2 2    S32G QSPI Nor镜像布局说明... 3 2.1  S32G Linux BSP对QSPI Nor启动的支持情况... 3 2.2  S32G  Yocto fsl-image-flash机制分析... 5 2.3  S32G QSPI Nor启动的镜像布局和修改目标... 7 3    镜像修改与编译... 8 3.1  镜像修改... 8 3.2  Yocto编译方法... 10 3.3  Standalong编译方法... 11 4    如何缩小Linux内核镜像... 12 5    如何制造最小Rootfs. 12 5.1  基于现有rootfs直接缩小... 12 5.2  其它方法... 14 6    测试... 14 6.1  烧写办法... 14 6.2  运行log. 16 7    如何在Rootfs加入应用... 17 7.1  Yocto环境中加入方法... 17 7.2  其它方法... 17 7.3  测试结果... 17 8    附件... 17    
View full article
本文说明如何检查S32DS Flash Tool的默认波特率,以便确认下载相关的失败问题,以及如何解决。 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 4 2    S32G波特率设置说明... 4 3    检查FlashTool Target image的默认波特率... 6 3.1  运行FlashTool下载Target image. 6 3.2  连接lauterbach检查波特率相关配置... 6 4    G2的检查情况... 8 5    如何解决此问题... 9  
View full article
this doc explain how to support high baudrate, such as 3M, 4M in S32G Mcore, even MCAL currently just support 1.8M. and to change uart clock source to avoid the wrongbaudrate value. and after that, still need modify the linux clock tree. 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 3 2    S32G波特率设置说明... 4 3    创建UART工程... 7 3.1  打开工程... 7 3.2  修改波特率... 7 3.3  编译与运行... 7 3.4  默认工程说明... 8 4    配置UART更高波特率... 9 4.1  以PERIPH_PLL_PHI3_CLK 100Mhz为LIN_CLK时钟源    9 4.2  以FIRC_CLK 48Mhz为LIN_CLK时钟源... 14 5    Linux的修改... 15 5.1  以PERIPH_PLL_PHI3_CLK 100Mhz为LIN_CLK时钟源    15 5.2  以FIRC_CLK 48Mhz为LIN_CLK时钟源... 19
View full article
UPDATE: I recommend trying the steps outlined in this NXP Community post first.     If we flash a RD-RW612-BGA binary into FRDM-RW612 the board will be locked, and we will no longer be able to write data into the flash until we unlock it. The reason why it locks is because the Winbond flash on the FRDM board has a lock bit that is enabled when flashing the RD application. Fortunately, there is a way to unlock it with the FlexSPI interface. In this document we will briefly show how to do this. In SDK 2.16.100, we will modify the frdmrw612_flexspi_nor_dma_tranfer SDK example. We're going to modify app.h, flexspi_nor_flash_ops.c and flexspi_nor_dma_transfer.c.   In app.h we modify/add some macros with the following values:       #define SECTOR_SIZE 0x10000 /* 64K */ #define NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD 0 #define NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG1 1 #define NOR_CMD_LUT_SEQ_IDX_WRITEENABLE 2 #define NOR_CMD_LUT_SEQ_IDX_ERASESECTOR 3 #define NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG2 4 #define NOR_CMD_LUT_SEQ_IDX_ERASECHIP 5 #define NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG3 6 #define NOR_CMD_LUT_SEQ_IDX_READ_NORMAL 7 #define NOR_CMD_LUT_SEQ_IDX_READID 8 #define NOR_CMD_LUT_SEQ_IDX_WRITE 9 #define NOR_CMD_LUT_SEQ_IDX_READSTATUSREG1 10 #define NOR_CMD_LUT_SEQ_IDX_READSTATUSREG2 11 #define NOR_CMD_LUT_SEQ_IDX_READSTATUSREG3 12 #define NOR_CMD_LUT_SEQ_IDX_READ_FAST 13 #define NOR_CMD_LUT_SEQ_IDX_ENABLE_RESET 14 #define NOR_CMD_LUT_SEQ_IDX_RESET_DEVICE 15 #define CUSTOM_LUT_LENGTH 64 /* Enable quad and update dummy cycle */ #define FLASH_QUAD_ENABLE 0xC740       Moving to flexspi_nor_flash_ops.c we will add/modify the following parameters: In flexspi_nor_wait_bus_busy(FLEXSPI_Type *base):     flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_READSTATUSREG1;       Right after the previous function we are going to add these new functions:     status_t flexspi_nor_write_status1(FLEXSPI_Type *base, uint8_t status1) { flexspi_transfer_t flashXfer; status_t status; uint32_t writeValue = status1; /* Make sure external flash is not in busy status. */ status = flexspi_nor_wait_bus_busy(base); if (status != kStatus_Success) { return status; } /* Write enable */ status = flexspi_nor_write_enable(base, 0); if (status != kStatus_Success) { return status; } /* Write the status register 1 */ flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Write; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG1; flashXfer.data = &writeValue; flashXfer.dataSize = 1; status = FLEXSPI_TransferBlocking(base, &flashXfer); if (status != kStatus_Success) { return status; } status = flexspi_nor_wait_bus_busy(base); /* Do software reset. */ #if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \ defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK) base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK; base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK); #else FLEXSPI_SoftwareReset(base); #endif return status; } status_t flexspi_nor_write_status2(FLEXSPI_Type *base, uint8_t status2) { flexspi_transfer_t flashXfer; status_t status; uint32_t writeValue = status2; /* Make sure external flash is not in busy status. */ status = flexspi_nor_wait_bus_busy(base); if (status != kStatus_Success) { return status; } /* Write enable */ status = flexspi_nor_write_enable(base, 0); if (status != kStatus_Success) { return status; } /* Write the status register 1 */ flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Write; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG2; flashXfer.data = &writeValue; flashXfer.dataSize = 1; status = FLEXSPI_TransferBlocking(base, &flashXfer); if (status != kStatus_Success) { return status; } status = flexspi_nor_wait_bus_busy(base); /* Do software reset. */ #if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \ defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK) base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK; base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK); #else FLEXSPI_SoftwareReset(base); #endif return status; } status_t flexspi_nor_write_status3(FLEXSPI_Type *base, uint8_t status3) { flexspi_transfer_t flashXfer; status_t status; uint32_t writeValue = status3; /* Make sure external flash is not in busy status. */ status = flexspi_nor_wait_bus_busy(base); if (status != kStatus_Success) { return status; } /* Write enable */ status = flexspi_nor_write_enable(base, 0); if (status != kStatus_Success) { return status; } /* Write the status register 1 */ flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Write; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG3; flashXfer.data = &writeValue; flashXfer.dataSize = 1; status = FLEXSPI_TransferBlocking(base, &flashXfer); if (status != kStatus_Success) { return status; } status = flexspi_nor_wait_bus_busy(base); /* Do software reset. */ #if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \ defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK) base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK; base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK); #else FLEXSPI_SoftwareReset(base); #endif return status; }   In  status_t flexspi_nor_enable_quad_mode(FLEXSPI_Type *base):     flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG1;                   Delete status_t flexspi_nor_flash_program(FLEXSPI_Type *base, uint32_t dstAddr, const uint32_t *src, uint32_t length) & status_t flexspi_nor_flash_page_program(FLEXSPI_Type *base, uint32_t dstAddr, const uint32_t *src).     Modify status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId) to:         status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId, uint16_t *deviceId)           Right after status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId, uint16_t *deviceId):         status_t flexspi_nor_get_status1(FLEXSPI_Type *base, uint8_t *status1) { uint32_t temp; flexspi_transfer_t flashXfer; flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Read; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_READSTATUSREG1; flashXfer.data = &temp; flashXfer.dataSize = 1; status_t status = FLEXSPI_TransferBlocking(base, &flashXfer); *status1 = temp; /* Do software reset or clear AHB buffer directly. */ #if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \ defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK) base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK; base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK); #else FLEXSPI_SoftwareReset(base); #endif return status; } status_t flexspi_nor_get_status2(FLEXSPI_Type *base, uint8_t *status2) { uint32_t temp; flexspi_transfer_t flashXfer; flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Read; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_READSTATUSREG2; flashXfer.data = &temp; flashXfer.dataSize = 1; status_t status = FLEXSPI_TransferBlocking(base, &flashXfer); *status2 = temp; /* Do software reset or clear AHB buffer directly. */ #if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \ defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK) base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK; base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK); #else FLEXSPI_SoftwareReset(base); #endif return status; } status_t flexspi_nor_get_status3(FLEXSPI_Type *base, uint8_t *status3) { uint32_t temp; flexspi_transfer_t flashXfer; flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Read; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_READSTATUSREG3; flashXfer.data = &temp; flashXfer.dataSize = 1; status_t status = FLEXSPI_TransferBlocking(base, &flashXfer); *status3 = temp; /* Do software reset or clear AHB buffer directly. */ #if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \ defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK) base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK; base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK); #else FLEXSPI_SoftwareReset(base); #endif return status; } status_t flexspi_nor_reset_device(FLEXSPI_Type *base) { status_t status; flexspi_transfer_t flashXfer; flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Command; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_ENABLE_RESET; status = FLEXSPI_TransferBlocking(base, &flashXfer); if (status != kStatus_Success) { return status; } status = flexspi_nor_wait_bus_busy(base); flashXfer.deviceAddress = 0; flashXfer.port = FLASH_PORT; flashXfer.cmdType = kFLEXSPI_Command; flashXfer.SeqNumber = 1; flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_RESET_DEVICE; status = FLEXSPI_TransferBlocking(base, &flashXfer); if (status != kStatus_Success) { return status; } status = flexspi_nor_wait_bus_busy(base); return status; }     Then in the last file flexspi_nor_dma_transfer.c:   We are modifying the prototype flexspi_nor_get_vendor_id to:     extern status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId, uint16_t *deviceId);     And we are going to add the following prototypes:     extern status_t flexspi_nor_get_status1(FLEXSPI_Type *base, uint8_t *status1); extern status_t flexspi_nor_get_status2(FLEXSPI_Type *base, uint8_t *status2); extern status_t flexspi_nor_get_status3(FLEXSPI_Type *base, uint8_t *status3); extern status_t flexspi_nor_reset_device(FLEXSPI_Type *base); extern status_t flexspi_nor_write_status1(FLEXSPI_Type *base, uint8_t status1); extern status_t flexspi_nor_write_status2(FLEXSPI_Type *base, uint8_t status2); extern status_t flexspi_nor_write_status3(FLEXSPI_Type *base, uint8_t status3); extern status_t flexspi_nor_erase_chip(FLEXSPI_Type *base);       In flexspi_device_config_t deviceconfig modify the following:     .dataValidTime = 2,     Modify the const uint32_t customLUT[CUSTOM_LUT_LENGTH] as follows:     const uint32_t customLUT[CUSTOM_LUT_LENGTH] = { /* Normal read mode -SDR */ [4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x13, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20), [4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL + 1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Fast read mode - SDR */ [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x0C, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20), [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST + 1] = FLEXSPI_LUT_SEQ( kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x0A, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Fast read quad mode - SDR */ [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xEC, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x20), [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD + 1] = FLEXSPI_LUT_SEQ( kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x0A, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04), /* Write Enable */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Erase Sector */ [4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x21, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20), /* Read ID */ [4 * NOR_CMD_LUT_SEQ_IDX_READID] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9F, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Write status 1 */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04), /* Write status 2 */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG2] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x31, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04), /* Write status 3 */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG3] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x11, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04), /* Dummy write, do nothing when AHB write command is triggered. */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITE] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x0, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x0), /* Read status 1 register */ [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x05, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Read status 2 register */ [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG2] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x35, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Read status 3 register */ [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG3] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x15, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Erase whole chip */ [4 * NOR_CMD_LUT_SEQ_IDX_ERASECHIP] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xC7, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Enable reset */ [4 * NOR_CMD_LUT_SEQ_IDX_ENABLE_RESET] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x66, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Reset device */ [4 * NOR_CMD_LUT_SEQ_IDX_RESET_DEVICE] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x99, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), };       In int main(void) add the following variables:     uint16_t deviceID = 0; uint8_t status1 = 0, status2 = 0, status3 = 0;         in main, configure the DMAMUX as follows (this should be before DMA_Init(EXAMPLE_DMA):     /* Configure DMAMUX. */ RESET_PeripheralReset(kINPUTMUX_RST_SHIFT_RSTn); INPUTMUX_Init(INPUTMUX); INPUTMUX_AttachSignal(INPUTMUX, EXAMPLE_TX_CHANNEL, kINPUTMUX_FlexspiTxToDma0); INPUTMUX_AttachSignal(INPUTMUX, EXAMPLE_RX_CHANNEL, kINPUTMUX_FlexspiRxToDma0); /* Enable trigger. */ INPUTMUX_EnableSignal(INPUTMUX, kINPUTMUX_Dmac0InputTriggerFlexspiRxEna, true); INPUTMUX_EnableSignal(INPUTMUX, kINPUTMUX_Dmac0InputTriggerFlexspiTxEna, true); /* Turnoff clock to inputmux to save power. Clock is only needed to make changes */ INPUTMUX_Deinit(INPUTMUX);       in main, delete all the code from PRINTF("\r\nFLEXSPI dma example started!\r\n"); to one line before the last while(1). Before that while, add the following code:   PRINTF("\r\nFLEXSPI Unlock code started!\r\n"); /* FLEXSPI init */ flexspi_nor_flash_init(EXAMPLE_FLEXSPI); /* Get vendor ID. */ status = flexspi_nor_get_vendor_id(EXAMPLE_FLEXSPI, &vendorID, &deviceID); if (status != kStatus_Success) { PRINTF("Error getting flash ids: 0x%x\r\n", status); return status; } PRINTF("Vendor ID: 0x%x\r\n", vendorID); PRINTF("Device ID: 0x%x\r\n", deviceID); /* Get Status 1 */ status = flexspi_nor_get_status1(EXAMPLE_FLEXSPI, &status1); if (status != kStatus_Success) { PRINTF("Error getting status1: 0x%x\r\n", status); return status; } PRINTF("Status 1: 0x%x\r\n", status1); /* Get Status 2 */ status = flexspi_nor_get_status2(EXAMPLE_FLEXSPI, &status2); if (status != kStatus_Success) { PRINTF("Error getting status2: 0x%x\r\n", status); return status; } PRINTF("Status 2: 0x%x\r\n", status2); /* Get Status 3 */ status = flexspi_nor_get_status3(EXAMPLE_FLEXSPI, &status3); if (status != kStatus_Success) { PRINTF("Error getting status3: 0x%x\r\n", status); return status; } PRINTF("Status 3: 0x%x\r\n", status3); if(status2 & 0x01) { PRINTF("Error, The Flash Status register is locked! Disconnect and connect the board with the ISP button pressed to clear it and try again.\r\n"); return 0; } status1 = 0x00; status2 = 0x02; /* Write 0s to Status 1 */ status = flexspi_nor_write_status1(EXAMPLE_FLEXSPI, status1); if (status != kStatus_Success) { PRINTF("Error writing status1: 0x%x\r\n", status); return status; } /* Write 0x02 (Quad enabled only) to Status 2 */ status = flexspi_nor_write_status2(EXAMPLE_FLEXSPI, status2); if (status != kStatus_Success) { PRINTF("Error writing status2: 0x%x\r\n", status); return status; } /* Get Status 1 */ status = flexspi_nor_get_status1(EXAMPLE_FLEXSPI, &status1); if (status != kStatus_Success) { PRINTF("Error getting status1: 0x%x\r\n", status); return status; } PRINTF("Status 1: 0x%x\r\n", status1); /* Get Status 2 */ status = flexspi_nor_get_status2(EXAMPLE_FLEXSPI, &status2); if (status != kStatus_Success) { PRINTF("Error getting status2: 0x%x\r\n", status); return status; } PRINTF("Status 2: 0x%x\r\n", status2); PRINTF("Erasing the whole chip, it will take several minutes to complete. \r\n"); status = flexspi_nor_erase_chip(EXAMPLE_FLEXSPI); if (status != kStatus_Success) { PRINTF("Error erasing: 0x%x\r\n", status); return status; } PRINTF("Chip erased!\r\n");     Now we need to compile. But first, we need to link the application to RAM. Please right click on the project and go to Properties. in C/C++ Build go to Settings. In MCU Linker, select Managed Linker Script and check the Link application to RAM box. Apply and close.   Now compile the example in MCUXpresso. Once compiled, get the binary. Go to the Debug folder in the project, and you will see an .axf file. Right click on the file and select Binary Utilities > Create binary. Now, we need to modify that binary. Open you preferred binary editor and delete everything from 0x0 to 0x17FFFFFFF. The first address in the binary (0x0) must have the data from 0x18000000. Now we can flash the binary. We are going to do this with blhost. 2 USB C cables are needed. We are going to connect them via J10 and J8. But first we need to setup the board in ISP mode. Connect J8 to the PC. Press the ISP button (SW3) and with the button pressed connect the board via J10. In blhost run the following:     blhost -u 0x1fc9,0x0020 get-property 1     Disconnect and connect (J10) your board with the ISP button pressed. Now run the following (YOUR BINARY should be the path and file in which the binary is located):     blhost -u 0x1fc9,0x0020 -- fill-memory 0x20001000 0x4 0xC0100002 blhost -u 0x1fc9,0x0020 -- configure-memory 0x9 0x20001000 blhost -u 0x1fc9,0x0020 -- get-property 0x19 0x9 blhost -u 0x1fc9,0x0020 -- write-memory 0x20000000 <YOUR BINARY>.bin blhost -u 0x1fc9,0x0020 -- execute 0x2000026c 0x20000000 0x20120000     If the above steps were correct, you should be able to flash your board again. Please try with a hello world example in MCUXpresso.
View full article
this doc explain the S32G PCIe HW design checkpoints and How to debug HW issue with SW. 主要包括:         1:S32G PCIe硬件设计说明。         2:如何根据硬件设计配置软件。         3:如何根据软件现象debug硬件连接问题。         4:一个连接PCIe外设的demo. 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 2 2    PCIe硬件设计说明... 2 2.1  S32G PCIe能力... 2 2.2  S32G PCIe原理图设计... 4 2.3  S32G PCIe设计说明... 8 2.4  S32G PCIe硬件bring up. 9 3    PCIe 软件说明... 9 3.1  软件配置说明... 9 3.2  PCIe uboot初始化流程... 12 3.3  PCIe Linux初始化流程... 19 4    硬件连接错误的软件表现示例... 21 4.1  时钟配置错误... 21 4.2  硬件连接错误... 23 5    RDB3连接PCIe设置Demo. 25 5.1  硬件说明... 25 5.2  Uboot配置... 26 5.3  内核打印... 27 5.4  内核sys文件夹... 36  
View full article
  Demo Owner Mike Stanley   Tire Pressure Monitoring Systems (TPMS) help drivers with precise direct tire pressure measurement by providing individual tire readings – including the spare. NXP's world’s smallest, lowest-power, with highest memory for customer use TPMS is highly integrated with a pressure sensor, temperature sensor, accelerometer, MCU and a transmitter. Watch Mike Stanley explain the pressure sensor readings, temperature sensor display and the accelerometer/motion readings. These readings are time based periodic measurements where the data is given as an output to the driver.   Features Simulation that portraits the TPMS as if it were inside the vehicles tires and sending reports to the vehicle's display unit about tire pressure Module has the following: Pressure sensor, accelerometer, temperature sensor, low-frequency radio, Microcontroller   Featured NXP Products FXTH87 product page FXTH87 Fact Sheet Links Tire Pressure Monitoring Sensors Pressure Sensors Block Diagram  
View full article
Some common issues of HSE-H based on S32G are summarized. Hope it can help you understand the known issues of HSE-H. The issue contents have been listed to facilitate finding the topic you care about. Please refer to the attachment for details. Thank you.
View full article
doc&patch explain how to decrease the qspi init clock to avoid the spi read qspi id error in linux S32G Linux BSP初始化QSPI Nor时钟是默认200Mhz,但是JEDEC规范建议读QSPI Nor ID是使用SPI模式,低速时钟,所以默认BSP是有可能读ID不成功的,本文说明如何解决这个问题。 本文采用软件版本为Linux BSP43 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 2 2    Linux QSPI Nor驱动说明... 3 2.1  QSPI Nor控制器驱动说明... 3 2.2  QSPI Nor设备驱动说明... 4 2.3  SPI Mem驱动说明... 5 3    代码修改... 6 3.1  将初始化时钟切换成133Mhz. 6 3.2  在初始化后将时钟切换回200Mhz. 7 4    测试... 7 4.1  软件测试... 7 4.2  硬件测量... 7 5    其它注意事项... 8    
View full article
This doc explain how to support RGMII/RMII/MII 100Mbps device in Mcal, and also the debug suggestion. in Chinese version. 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 2 2    RGMII RMII MII区别说明... 2 2.1  IO管脚与信号方向... 2 2.2  时钟说明... 7 2.3  注意事项... 7 3    RGMII MCAL配置... 8 3.1  MCAL配置... 8 3.2  注意事项... 10 4    RMII MCAL配置... 11 4.1  MCAL配置... 11 4.2  注意事项... 13 5    MII MCAL配置... 14 5.1  MCAL配置... 14 5.2  注意事项... 15 6    其它建议... 16 6.1  Debug. 16 6.2  EMI 16  
View full article
Chinese version   S32G的partition off流程要求核稳定的进 入到WFI状态,本文说明如何修改Linux内核, 在A53 Linux关机或kernel panic时,如何让所 有A53 Core进入WFI。 目录 1 背景说明与参考资料 .................................................. 2 1.1 背景说明 ................................................................. 2 1.2 参考资料 ................................................................. 5 1.3 测试工具 ................................................................. 6 2 Panic ......................................................................... 7 2.1 Panic代码流程分析 ................................................. 7 2.2 BSP30修改说明(Non-ATF) ................................... 10 2.3 BSP36修改说明(ATF) .......................................... 15 3 Poweoff ................................................................... 17 3.1 Poweroff代码流程分析 ......................................... 17 3.2 BSP30修改说明(Non-ATF) ................................... 19 3.3 BSP36修改说明(ATF) .......................................... 20 4 Reboot情况说明 ....................................................... 20 5 STR情况说明 ........................................................... 21   Contents 1    Background and Reference. 2 1.1  Background. 2 1.2  Reference materials. 5 1.3  Test Tools. 6 2    Panic. 7 2.1  Panic code flow analysis. 7 2.2  BSP30 Modification (Non-ATF) 10 2.3  BSP36 Modification (ATF) 16 3    Poweoff 18 3.1  Poweroff code analysis. 18 3.2  BSP30 Modification (Non-ATF) 20 3.3  BSP36 Modification (ATF) 21 4    Reboot Description. 21 5    STR Description. 21
View full article
本文说明在S32G上,如何升高以太网MDIO总线速度,其应用场景主要是为了提高MDIO的访问速度,来应对S32G对外部交换机的高速诊断要求,因为通常外部交换机可以支持高速MDIO。 本文说明方法并不保证信号质量和符合规范,请注意。 目录 1    需要的资料... 2 2    背景说明... 2 3    硬件说明... 3 4    PFE MCAL驱动代码修改... 4 4.1  MDIO时钟树说明... 4 4.2  创建PFE MCAL Master工程... 7 4.3  MDIO源代码说明... 7 4.4  源代码修改... 7 4.5  测试... 8 5    PFE Linux驱动修改说明(未测试) 9
View full article
doc&project&patch&script explain to support GD qspi nor in lauterbach, flash tool,ivt,fls mcal, fls bootloader and linux/ chinese/english 目录 1    背景和参考资料... 2 1.1  背景说明... 2 1.2  参考资料... 3 1.3  硬件连接... 5 2    Lauterbach脚本驱动开发(可选) 5 2.1  准备参考脚本... 5 2.2  QuadSPI_ReadID.. 6 2.3  配置QSPI NOR为DOPI模式... 7 2.4  使用DOPI模式 READ_8DTRD.. 10 2.5  测试结果... 13 3    Flash tool算法镜像开发... 14 3.1  Flash SDK实现的算法... 15 3.2  开发新的flash源代码... 17 3.3  测试结果... 20 4    开发IVT参数头... 22 4.1  S32G QSPI控制器配置区别... 24 4.2  QSPI的配置区别... 28 4.3  测试结果... 29 5    开发MCAL Fls驱动... 30 5.1  MCAL Fls驱动工程说明... 30 5.2  FlsMem配置页... 34 5.3  MemCfg配置页... 35 5.4  测试结果... 49 6    开发Bootloader工程中Fls驱动... 51 6.1  Bootloader工程说明... 51 6.2  Bootloader与MCAL Fls驱动的不同点... 53 6.3  镜像打包... 54 6.4  测试结果... 56 7    开发Linux驱动(可选) 57 7.1  Linux GD驱动支持情况... 57 7.2  时钟相关的修改... 58 7.3  在DTS中增加GD flash的支持... 60 7.4  修改源代码增加flash信息结构体... 61 7.5  修改源代码中flash的fixup支持DTR模式... 62 7.6  Turning dummy值解决读错位的问题... 64 7.7  测试结果... 65   Content 1    Background and References. 2 1.1  Background. 2 1.2  References. 3 1.3  Hardware Link. 5 2    Lauterbach Script development(Optional) 6 2.1  Preparing the refer script 6 2.2  QuadSPI_ReadID.. 6 2.3  Configure QSPI NOR to DOPI mode. 8 2.4  Use DOPI mode  READ_8DTRD.. 11 2.5  Test report 13 3    Flash tool algorithm image development 15 3.1  Algorithms implemented by Flash SDK. 15 3.2  Develop new flash source code. 17 3.3  Test Report 21 4    Develop IVT Parameter Header 23 4.1  S32G QSPI Controllder configuration difference. 25 4.2  QSPI Configuration Difference. 30 4.3  Test Report 30 5    Develop MCAL Fls driver 31 5.1  MCAL Fls Driver Project Details. 31 5.2  FlsMem Configuration page. 35 5.3  MemCfg Configuration page. 36 5.4  Test Report 51 6    Develop Bootloader Project Fls Drivedr 52 6.1  Bootloader Project Details. 52 6.2  Difference of Bootloader and MCAL Fls Driver 54 6.3  Image Package. 56 6.4  Test Report 58 7    Develop Linux Driver(Optional) 59 7.1  Linux GD Driver Details. 59 7.2  Modification of Clock. 60 7.3  In DTS add GD flash Support 62 7.4  Modify source code and add flash information structure  63 7.5  Modify the fixup of flash in source code to support DTR mode  64 7.6  Turning Dummy Value to Solve the Misplacement Problem   66 7.7  Test Report 67
View full article
本文说明在S32G3 RDB3板上,Uboot中使能PFE驱动时,需要加载PFE FW,默认Uboot中,PFE FW是放在SD/eMMC的FAT分区,通过文件系统访问来读取。本文说明如何修改为从QSPI NOR中读取。主要的应用场景是:  在烧写镜像时,需要Uboot通过网口来烧写内核镜像及rootfs。而此时SD/eMMC还没有分区,所以无法将PFE网口需要的FW放在FAT分区中。 目录 1    背景与相关资料... 2 1.1  问题背景... 2 1.2  需要的软件,工具与文档... 3 2    将Uboot PFE FW放在QSPI Nor上... 4 2.1  Uboot代码说明与修改... 4 2.2  测试... 6
View full article
本文说明在S32G上如何修改eMMC时钟,来避开200Mhz的或及倍频的频率EMI干扰检查点。 目录 1    背景说明和需要的资料... 2 1.1  背景说明... 2 1.2  需要的资料... 2 2    eMMC的硬件连接... 3 3    eMMC时钟初始化方法... 4 3.1  eMMC时钟源说明及修改目标... 4 3.2  M7+Bootloader方法(可选项) 6 3.3  ATF初始化方法... 7 4    修改eMMC时钟... 9 4.1  ATF的修改... 9 4.2  Uboot相关的修改... 9 4.3  非整除时钟的修改考虑... 10 5    测试结果... 11 update to V2,增加分数分频: 6    分数分频... 13 6.1  调试方法... 13 6.2  代码修改... 14 6.3   测试结果   15
View full article
本文说明S32G在Linux中如何使用内存读写工具来发起一个HSE Server服务请求,以确认HSE是否正常工作。本说明的目的旨在在极端缺少Debug手段的情况下,确认HSE的状态。 目录 1    背景说明与参考资料... 2 1.1  背景说明... 2 1.2  参考资料... 2 2    启动包含HSE的Linux镜像... 3 3    HSE服务代码逻辑与寄存器状态... 3 3.1  HSE Demo示例... 3 3.2  IDEL情况下MU寄存器状态... 6 4    使用Linux memtool命令来访问HSE. 10 4.1  检查HSE状态... 10 4.2  准备hseSrvDescriptor_t数据结构... 10 4.3  申请HSE服务... 11 5    其它建议... 12
View full article
本文说明如何配置MCAL UART模块为DMA模式。 默认的MCAL UART模块是使用的PIO模式。 本文采用软件版本为MCAL RTD 4.0.2。 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 2 2    创建UART工程... 2 2.1  打开工程... 2 2.2  修改波特率... 3 2.3  编译... 3 2.4  默认工程说明与运行... 4 3    配置UART DMA模式... 5 3.1  参考资料... 5 3.2  增加并配置MCL模块... 5 3.3  修改UART模块... 6 3.4  修改Platform模块... 7 3.5  处理Cache相关问题... 7 3.6  测试结果... 8
View full article
本文说明如何配置MCAL ICU模块为GPIO Input。 默认的MCAL ICU模块是使用FTM输入为示例的。 本文采用软件版本为MCAL RTD 4.0.2 目录 1    背景与资料说明... 2 1.1  背景说明... 2 1.2  所需资料说明... 2 2    创建ICU工程... 3 2.1  打开工程... 3 2.2  编译与运行... 3 2.3  默认工程说明... 4 3    增加GPIO输入支持... 6 3.1  修改说明... 6 3.2  修改Port模块... 6 3.3  修改ICU模块... 7 3.4  Platform模块... 8 3.5  主测试程序修改... 9 3.6  测试结果... 10
View full article
本文说明S32G3 M7核Standby MCAL demo 详细情况及定制,并在进入Standby之前 调用QSPI 接口将QSPI NOR flash配置进入 deep power down模式,以节省用电。 目录 1    参考资料说明... 2 2    G2和G3 Demo的区别... 2 3    G3 MCAL Demo的实现... 4 3.1  修改UART驱动... 4 3.2  实现时钟关闭代码... 4 3.3  配置电源模式切换驱动... 5 3.4  配置唤醒源... 5 3.5  加入PMIC驱动... 6 3.6  主函数逻辑实现... 7 3.7  运行测试... 7 3.8  未来开发计划... 8 4    将QSPI NOR设置进入Deep Power Down模式... 8 4.1  Fls层的修改... 10 4.2  中间层的修改... 10 4.3  QSPI_IP层的修改... 13 4.4  主测试函数调用... 16 4.5  Fls驱动的测试... 17 5    将Deep Power Down功能集成到STANDBY工程中并测试    18 5.1  EB配置... 18 5.2  主测试函数与编译修改... 20 5.3  运行测试... 21
View full article
现在越来越多的客户,对于S32G PFE在master/slave的使用有了需求。 但是,PFE只有4个HIF接口,HIF0~HIF3,而PFE有3个EMAC口,以及LLCE2PFE也需要要给HIF,从而HIF成为一个关键资源。 同时,有些客户需要从A核,M核的业务考量,A核和M核的网络不仅要和外部设备进行通信,同时A核和M核内部也有通信需求,并且需要把业务报文和管理报文分离,这就对PFE master/slave的使用场景有了更多变化,以及对各种配置有了更多需求。 因此,针对PFE/Slave的几种使用典型的使用场景,进行配置。
View full article
在进行时钟同步时,目前S32G2/G3有一种很典型的使用场景: Grand master clock  <-> S32G PFE <-> 其余连接在PFE 某些 eMAC口上的设备 外部的grand master clock,连接在PFE的一个eMAC上,要同步S32G以及连接在PFE其余eMAC上的设备时钟。 但是S32G2/G3的PFE仅仅是支持timestamp,对于将S32G PFE设置成交换机使用时,PFE不能实现Transparent clock的功能。 因此,本文讨论将PFE + S32G SoC当作Transparent clock,以及将PFE + S32G当作boundary clock,来同步S32G以及其余部件的时钟。
View full article