S32G PFE master/slave scenarios configurations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G PFE master/slave scenarios configurations

S32G PFE master/slave scenarios configurations

现在越来越多的客户,对于S32G PFE在master/slave的使用有了需求。

但是,PFE只有4个HIF接口,HIF0~HIF3,而PFE有3个EMAC口,以及LLCE2PFE也需要要给HIF,从而HIF成为一个关键资源。

同时,有些客户需要从A核,M核的业务考量,A核和M核的网络不仅要和外部设备进行通信,同时A核和M核内部也有通信需求,并且需要把业务报文和管理报文分离,这就对PFE master/slave的使用场景有了更多变化,以及对各种配置有了更多需求。

因此,针对PFE/Slave的几种使用典型的使用场景,进行配置。

Labels (1)
Attachments
100% helpful (1/1)
Version history
Last update:
‎03-05-2024 07:44 PM
Updated by: