eBike and Industrial Motor Control with Kinetis E MCU and MC34937 Motor Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eBike and Industrial Motor Control with Kinetis E MCU and MC34937 Motor Driver

eBike and Industrial Motor Control with Kinetis E MCU and MC34937 Motor Driver

Explore the MC34937, an industrial-grade 3-phase gate pre-driver for BLDC and PMSM motor control. The MC34937 can support 12V, 24V, and 36V motor control applications and easily interfaces to standard MCUs and DSPs. The demo shows the implementation of the MC34937 with Kinetis Microcontrollers E in a 36V battery-operated electric bike (eBike) application. This same system can be modified to be used in other industrial applications such as electric garden tools, industrial fans and pumps, and electric wheelchairs.

Features
  • Demo shows capability of Kinetis KE02 connecting to an MC34937 Motor Driver
  • MC34937 able to drive 12V, 24V, 36V, 48V systems

Featured NXP Products


Block Diagram

Capture.JPG.jpg

MC34937

Capture.JPG.jpg

Schematics and Software:

ラベル(1)
添付
コメント

Customer is interested on this reference and checking with us who is the supplier for motor and battery used in this reference. This will help them to speed design using the reference. 

Thanks.

Regards,

Audrey

Hello
Do you know  who is the supplier for motor? This board is avaible to buy or i have to make all if i want a system like that?
thanks

Jean Pierre

評価なし
バージョン履歴
最終更新日:
‎07-07-2014 01:42 PM
更新者:
NXP Employee