Machine Learning and Sensor Data Analytics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Machine Learning and Sensor Data Analytics

Machine Learning and Sensor Data Analytics

Smart Pump Monitor Demo

This demo shows a small water pump rig consisting of a water pump and 3 valves put together to collect data for supervised machine learning. Normal operation as well as abnormal conditions may be simulated with the rig. There are 2 sensor boards attached by clamps to the water pipe. Each sensor board has many sensors on it, but only the accelerometer will be used to gather the data. One board is used for data logging.  The other runs a model which was generated via machine learning based on data logged from the first board.  Pump vibration measurements are processed through the model by the MCU on that board to determine the operating state of the system

Features

  • Use of accelerometer to measure pipe vibration
  • Sensing algorithm detects when the pump is clogged or drawing on air
  • How to find patterns in data taken by NXP Sensors

Links

Related demos

Labels (1)
Comments

We are providing the Best Data Science Course Training Institute in Pune with Job assistance & offers a blended model of data science training. It helps you to master in Python, ML, Git, etc. to become a certified Data Scientist. Enroll in the best training now!

 

Data Science Course in Pune

No ratings
Version history
Last update:
‎07-07-2016 12:40 PM
Updated by:
NXP Employee