FAQ based on S32G HSE-H

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FAQ based on S32G HSE-H

FAQ based on S32G HSE-H

Some common issues of HSE-H based on S32G are summarized. Hope it can help you understand the known issues of HSE-H.

The issue contents have been listed to facilitate finding the topic you care about. Please refer to the attachment for details. Thank you.

 

HSE FW Attributes

  • Q: When is power on VDD_EUFSE required ?
  • Q: Why does the HSE self-test fail in HSE FW 1.0.5
  • Q: How to sign for serial bootloader
  • Q: Which data of SYS_IMG will be verified during boot phase
  • Q: What is SIMULATED_OEM/IN_FEILD attribute and how to use it?
  • Q: Where can I check the anti-rollback counter numbers in FW_IMG* and SYS_IMG?
  • Q: How does HSE allocate time slots if there are multiple service requests?
  • Q: What are heavy operations and what are fast operations?
  • Q: What to do if a fatal error occurs (GSR bit 16 to bit 31 non-zero)?
  • Q: What do those fatal errors in GSR stand for?
  • Q: Can we verify the Blue image offline?
  • Q: Is anti-rollback protection enabled by default?
  • Q: What is random IV number
  • Q: Is it feasible to format the key catalog in SYS_IMG when LC=IN_FEILD?
  • Q: Does FSR and GSR have same value for each MUs?

Boot

  • Q: Boot flow
  • Q: Secure boot
  • Q: If IVT_AUTH==1, can BOOT_SEQ keep to non-secure boot(BOOT_SEQ==0)
  • Q: What may cause secure boot fail

HSE FW Service

  • Q: Why some services are taking longer times than usual
  • Q: How often is the RNG reseeded
  • Q: Which services may include RNG reseeding?
  • Q: Does HSE UIO support suspend&resume?
  • Q: How to export derive keys
  • Q: Which key usage flags have conflict
  • Q: How to import keys that crypto driver doesn’t support?

HSE FW Others

  • Q: How to power VDD_EFUSE
  • Q: Why should XRDC give HSE the access to  NCSPD_STAT register
  • Q: What should be done before Life_Cycle advancement?
  • Q: Why can't the 1.0.9 HSE demo load SYS_IMG with QSPI reconfiguration parameters when non-secure boot?
  • Q: Which peripherals’ access should be given to HSE in XRDC configuration?
  • Q: Why do we recommend switching HSE FW from pink to blue?

 

标签 (1)
附件
无评分
版本历史
最后更新:
‎08-06-2025 12:11 PM
更新人: