Cloud-Connected Parking Spot Sensor - LS1021

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cloud-Connected Parking Spot Sensor - LS1021

Cloud-Connected Parking Spot Sensor - LS1021

Cloud-Connected Parking Spot Sensor

Demo

This demo shows a use case of the LS1021 IoT GW along with a FRDM-KW24 powered Magnetometer sensor to monitor the  car parking spot  locations such as garage parking  in a building, Traffic Management and Traffic Monitoring   The data can be reported and monitored from the Cloud.

Features:

  • Small footprint platform with a wide variety of high-speed connectivity and low-speed serial interfaces through the use of the ARM-based QorIQ LS1021A embedded processor.
  • The  FRDM-KW2 sensor data is send via Thread to the LS1021 IoT GW and The Proximetry Agent posts information to cloud server.

_______________________________________________________________________________________________________

Featured NXP Products:

ProductLink
Freedom Development Platform for Kinetis® KW2x MCUsFRDM-KW24D512|Freedom Development Platform|Kinetis | NXP 
LS1021A-IoT Gateway Reference Designhttps://www.nxp.com/design/designs/ls1021a-iot-gateway-reference-design:LS1021A-IoT?&lang_cd=en

_______________________________________________________________________________________________________

148861_148861.pngpastedImage_23.png

N15

Labels (1)
Tags (3)
Comments

"FRDM-KW24 powered Magnetometer sensor to monitor the  car parking spot  locations"

Please can you provide a little bit more details on the used sensing principle and how the "parking lot" is designed/realized? Thank you.

edk

Hi Alexander, please check the following blogs talking about the subject:

Aswin Sivakumar 

No ratings
Version history
Last update:
‎05-06-2016 12:49 PM
Updated by: