Cloud Connected ECG Wearable using NXP’s Single Chip Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cloud Connected ECG Wearable using NXP’s Single Chip Module

Cloud Connected ECG Wearable using NXP’s Single Chip Module

The demo from FirstView Consultants is a wearable medical EKG alert with Wi-Fi connection to enable Cloud reporting and diagnosis. The demo consists of an SCM-i.MX 6SoloX V-Link device (i.MX6SoloX/PF0100/512MB LPDDR2) + Firstview V-Link Top board with 802.11 b/g/n, Bluetooth

 

 

SCM V-Link technology is ideal for handheld/space-constrained applications allowing customers to integrate vertically.

 

Features:

  • AFIB detection with diagnosis and report to Cloud via Wi-Fi.
  • Top board contains: Wi-Fi/BT module (802.11 b/g/n), NXP 6-axis sensor and SPI NOR Flash 1 GB.
  • Base SCM device: 15.5x15.5mm.

____________________________________________________________________________________________________

Featured NXP Products:

ラベル(1)
タグ(2)
添付
評価なし
バージョン履歴
最終更新日:
‎05-09-2016 03:28 PM
更新者:
NXP Employee