tda8024 for ISO7816-3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tda8024 for ISO7816-3

1,533 Views
hanjin_kim
Contributor I

I will use tda8024 or 8029 for t=0/t=1 protocol in ISO 7816-3 but according to AN10267, tda8024 is not compatible EMV.

However, according to datasheet of tda8024, It is compatible for ISO 7816 and EMV.

What is true?  

Tags (3)
0 Kudos
Reply
1 Reply

1,431 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hope you are doing great, can you please send me the link to that AN you mention. 

as you can see  in the Datasheet and in the application note for TDA8024  it is stated that the  TDA8024 is EMV compliant,  in  AN10141 in section 1 also in datasheet  section 2.  the one that is not recommended for this is the 8029  it is not compliant anymore for EMVco 4.3c. 

 please check this references and let me know if this helps.

BR

Jonathan

0 Kudos
Reply