tda8024 for ISO7816-3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tda8024 for ISO7816-3

1,532件の閲覧回数
hanjin_kim
Contributor I

I will use tda8024 or 8029 for t=0/t=1 protocol in ISO 7816-3 but according to AN10267, tda8024 is not compatible EMV.

However, according to datasheet of tda8024, It is compatible for ISO 7816 and EMV.

What is true?  

タグ(3)
0 件の賞賛
返信
1 返信

1,430件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hope you are doing great, can you please send me the link to that AN you mention. 

as you can see  in the Datasheet and in the application note for TDA8024  it is stated that the  TDA8024 is EMV compliant,  in  AN10141 in section 1 also in datasheet  section 2.  the one that is not recommended for this is the 8029  it is not compliant anymore for EMVco 4.3c. 

 please check this references and let me know if this helps.

BR

Jonathan

0 件の賞賛
返信