slix-s

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

slix-s

1,309 Views
kent
Contributor I

SLIX-S PRIVACY PROTECTION PASSWORD IS ERRO, I HAVE TRIED SAME LIKE SLI-S.

CAN YOU TELL ME WHAT IS THE RIGHT PROCEDURE OF PRIVACY PROTECTION PASSWORD.

0 Kudos
Reply
1 Reply

1,192 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

With SLI-S we need to set password first, with the -S and -L you have to send the password within the command itself – ENABLE PRIVACY - BAh(as with the SLIX 2). See datasheet.

  • All password bytes are 00h for the read and write protection password and the
    EAS/AFI password.
  •  All password bytes are 0Fh for the Privacy and Destroy passwords(Section 8.2.2 datasheet)

pastedImage_1.png

BR

Jonathan

0 Kudos
Reply