phFlashBoot_HwInit() problem of PN7462

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

phFlashBoot_HwInit() problem of PN7462

4,149 Views
raycai
Contributor I

Our customer use PN7462 for NFC reader, But the customer feedback, They have question of on SW_FW SDK(PN7462AU FW and SW Examples Full Version - v04_06_00), They found the SW will hang-up on phFlashBoot_HwInit() @ static void phFlashBoot_HwTearDown(void)  . On the customer HW circuit, They have not the TDA8026 part.

0 Kudos
Reply
2 Replies

3,940 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Ray,

So this is a custom board based on PN7462 , right? Which example was running on that board?


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,939 Views
raycai
Contributor I

Dear Kan,

The HW design by customer, I helping customer to review the HW, I think the HW seem has some issue. Let’s me check and reply you later.

Thanks for you support.

Ray Cai

[email protected]<mailto:%[email protected]>

Avnet Electronics Marketing

8/F,Block 2,Science Park Financial Base,8 Kefa Road, Hi-Tech Industrial Park, Nanshan, Shenzhen

深圳市南山区科技园科发路8号金融基地2栋8楼

M +86.18665998896

D +86 755 86342385

F +86 755 26544345 - 2385

avnet.com<http://avnet.com/>

发件人: Kan_Li

发送时间: 2017年4月11日 16:19

收件人: Cai, Ray <[email protected]>

主题: Re: - Re: phFlashBoot_HwInit() problem of PN7462

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: phFlashBoot_HwInit() problem of PN7462

reply from Kan_Li<https://community.nxp.com/people/Kan_Li?et=watches.email.thread> in NFC - View the full discussion<https://community.nxp.com/message/895816?commentID=895816&et=watches.email.thread#comment-895816>

0 Kudos
Reply