icode slix commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

icode slix commands

2,613件の閲覧回数
ronvis
Contributor I

Dear Friend,

I'm new to ISO15693 protocol.

Do you have a SDK for your SL2S2002 chip?

or do you have any example of GET RANDOM NUMBER command?

How calculation of CRC16 is done?

Thank you for your help

Ron.

0 件の賞賛
返信
3 返答(返信)

2,474件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Which reader are you using? This is to verify if we have something available.

What do you mean by how it's the calculation ? are you looking for implementation for your reader? 

Regards, 
Estephania  

0 件の賞賛
返信

2,474件の閲覧回数
ronvis
Contributor I

Hello,

I'm using MP30U reader/writer module from GIGA-TMS.

here is the answer i got from them: "Because your requested function (set password, lock password) is not ISO15693 standard command, it needs from NXP itself additional command.  It must apply the registration from NXP with expense, and then they will provide Datasheet to you.

If you need to develop this function, you will need to apply to NXP directly. "

i would like to set/get commands from a terminal application with the chip (that is way i asked for the CRC calculation).

Thank you,

Ron.

0 件の賞賛
返信

2,474件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

The only information about it it's the one on the web page of the part, we have some examples with our readers, nonetheless,  there are some of the documents and libraries which are under NDA (Non-Disclosure Agreement) and placed in Docstore, if you are interested on seeing them you please follow these guides?

Docstore tutorial part 1: User Registration|NXP 

Docstore tutorial part 2: portal usage|NXP 

Also, you will need to contact one of our distributors available in the Distributor Network | NXP  to help you through the NDA process.

Regards, 

Estephania 

0 件の賞賛
返信