iOS support for Originality Signature reading and verification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iOS support for Originality Signature reading and verification

952件の閲覧回数
HP009
Contributor I

Does iOS support Originality Signature reading in NTAG21x ICs ? if there is no direct command to do that, are there any methods to execute custom commands? I saw that iOS 13 supports custom commands for NFC type -v tags. Does it support custom commands for NFC type 2 tags (ISO14443) as well?

0 件の賞賛
返信
1 返信

940件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @HP009 ,

 

Actually it is an implementation topic on application level, just as other commands implementation in an iOS App such as NTAG I2C Demo App, please kindly refer to https://community.nxp.com/t5/NFC-Knowledge-Base/NTAG-I2C-Demo-iOS-source-code-sharing/ta-p/1225337?s... for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信