A. cockpit is not suitable to demonstrate the full nfc functions, i think:
- missing the p2p and hce(with ndef) UI pages,
- missing picc autopolling function (auto discovery)
- missing mifare, icode cards' demo UI pages.
B. Is there any plan to open the Reader Library for WinOS?
cockpit is based on NxpNfcRdLib.dll, but without proper c/c++ header and .lib files,
we cannot use eva-board on windows platform. but there is many _WIN32 macros
and a 'ph_NxpBuild_Pc.h' header.
my plan is, get to familiar with nfc reader library on windows msvc, and cutdown
the reader library to target mcu which resource is limited.
btw. it should be very wonderful, nxp reader library with python binding officially.
 
					
				
		
 estephania_mart
		
			estephania_mart
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
Thank you very much for the feedback provided I’ll pass it over to the corresponding team. About the second question , we currently do not have any plans to open the Reader Library for Windows.
Best Regards,
Estephania
Hello,
for the file "ph_NxpBuild_Pc.h", you can start by copying file "ph_NxpBuild_Platform.h" into file "ph_NxpBuild_Pc.h". Then you'll need to make some changes
Vincent