Will NfcFactoryTestApp detect RFID card in Continuous RF ON mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will NfcFactoryTestApp detect RFID card in Continuous RF ON mode

2,417件の閲覧回数
srinavamani
Contributor I

Hi,

I'm trying to integrate PN7150 with our prototype using Android 7.1.2 AOSP. I followed NXP NCI Android Porting Guidelines AN11690. Used NfcFactoryTestApp native application test the integration. I received following log. Help us in integrating pn7150 module with our android prototype.

1. What is the use of Continuous RF ON and RRBS mode? I tried showing RFID cards in Continuous RF mode. But, it doesn't show detect the card.

msm8909:/ # /data/NfcFactoryTestApp                                           

----------------------------
NFC Factory Test Application
----------------------------
PN7150 NFC controller detected
Select the test to run:
     1. Continuous RF ON
     2. PRBS
Your choice: 1
Continuous RF ON test
  NFC Controller is now in continuous RF ON mode - Press enter to stop

2. In Android Settings, NFC settings is in blocked mode. While trying to enable receiving following error message in logcat.

01-01 05:21:03.439  7258  7258 I NfcService: Starting NFC service
01-01 05:21:03.460  7258  7258 D BrcmNfcJni: JNI_OnLoad: enter
01-01 05:21:03.460  7258  7258 I BrcmNfcJni: NFC Service: loading nci JNI
01-01 05:21:03.460  7258  7258 D BrcmNfcJni: register_com_android_nfc_NativeNfcManager: enter
01-01 05:21:03.460  7258  7258 D BrcmNfcJni: PowerSwitch::initialize: level=PS-UNKNOWN (0)
01-01 05:21:03.460  7258  7258 D NfcAdaptation: bool CNfcConfig::readConfig(const char *, bool) Opened base config /etc/libnfc-brcm.conf
01-01 05:21:03.468  7258  7258 D NfcAdaptation: bool CNfcConfig::readConfig(const char *, bool) Opened optional config /etc/libnfc-nxp.conf
01-01 05:21:03.477  7258  7258 D NfcAdaptation: bool CNfcConfig::readConfig(const char *, bool) Cannot open config file /data/nfc/libnfc-nxpTransit.conf
01-01 05:21:03.477  7258  7258 D NfcAdaptation: const CNfcParam *CNfcConfig::find(const char *) const found SCREEN_OFF_POWER_STATE=(0x1)
01-01 05:21:03.477  7258  7258 D BrcmNfcJni: PowerSwitch::initialize: desired screen-off state=1
01-01 05:21:03.477  7258  7258 D BrcmNfcJni: register_com_android_nfc_NativeNfcManager: exit
01-01 05:21:03.478  7258  7258 D BrcmNfcJni: register_com_android_nfc_NativeNfcTag
01-01 05:21:03.479  7258  7258 D BrcmNfcJni: RoutingManager::RoutingManager():enter
01-01 05:21:03.479  7258  7258 D         : bool CNxpNfcConfig::readConfig(const char *, bool) Opened base config /etc/libnfc-nxp.conf
01-01 05:21:03.485  7258  7258 E         : bool CNxpNfcConfig::readConfig(const char *, bool) Cannot open config file /data/nfc/libnfc-nxpTransit.conf
01-01 05:21:03.485  7258  7258 D BrcmNfcJni: RoutingManager::RoutingManager():exit
01-01 05:21:03.485  7258  7258 D BrcmNfcJni: RoutingManager::registerJniFunctions
01-01 05:21:03.486  7258  7258 D BrcmNfcJni: JNI_OnLoad: exit
01-01 05:21:03.486  7258  7258 D BrcmNfcJni: nfcManager_initNativeStruc: enter
01-01 05:21:03.487  7258  7258 D BrcmNfcJni: nfcManager_initNativeStruc: exit
01-01 05:21:03.492  7258  7258 W Settings: Setting device_provisioned has moved from android.provider.Settings.Secure to android.provider.Settings.Global.
01-01 05:21:03.526  4148  4322 D HHC85xx_Service: Status = Reconnecting
01-01 05:21:03.561  7258  7258 W NfceeAccess: could not find /etc/nfcee_access.xml, no NFCEE access allowed
01-01 05:21:03.561  7258  7258 I NfceeAccess: read 0 signature(s) for NFCEE access
01-01 05:21:03.562  7258  7258 W NfcSccAccess: could not find /etc/nfcscc_access.xml, no NFCSCC access allowed
01-01 05:21:03.562  7258  7258 I NfcSccAccess: read 0 signature(s) for NFCSCC access
01-01 05:21:03.562  7258  7258 W NfcSeAccess: could not find /etc/nfcse_access.xml, no NFCSE access allowed
01-01 05:21:03.562  7258  7258 I NfcSeAccess: read 0 signature(s) for NFCSE access
01-01 05:21:03.568  7258  7258 D NfcService: Enforcing a policy change on user: UserHandle{0}, isActiveForUser = true
01-01 05:21:03.637  7258  7258 D AidRoutingManager: mDefaultRoute=0x0
01-01 05:21:03.637  7258  7258 D AidRoutingManager: mDefaultOffHostRoute=0x2
01-01 05:21:03.638  7258  7258 D AidRoutingManager: mAidMatchingSupport=0x0
01-01 05:21:03.638  7258  7258 D AidRoutingManager: mAidTableSize=0x0
01-01 05:21:03.640  7258  7258 D RegisteredT3tIdentifiersCache: RegisteredT3tIdentifiersCache
01-01 05:21:03.661  7258  7258 D RegisteredServicesCache: Dynamic AIDs file does not exist.
01-01 05:21:03.664  7258  7258 D RegisteredNxpServicesCache: readDynamicApduService End:   0
01-01 05:21:03.668  7258  7258 D RegisteredServicesCache:  Reading service state data always from file
01-01 05:21:03.670  7258  7258 D RegisteredServicesCache: ServiceStateFileVersion=1.0
01-01 05:21:03.670  7258  7258 E RegisteredServicesCache: Next Tag=services
01-01 05:21:03.671  7258  7258 E RegisteredServicesCache: 1invalidateCache:WriteServiceStateToFile
01-01 05:21:03.671  7258  7258 E RegisteredServicesCache:  Writing service state Data Always
01-01 05:21:03.796  7258  7258 D CardEmulationManager: Current default: null
01-01 05:21:03.797  7258  7258 D CardEmulationManager: No default set, last payment service removed.
01-01 05:21:03.797  7258  7258 D RegisteredAidCache: onServicesUpdated
01-01 05:21:03.798  7258  7258 D RegisteredAidCache: Not updating routing table because NFC is off.
01-01 05:21:03.799  7258  7258 D RegisteredNfcFServicesCache: Dynamic System Code, NFCID2 file does not exist.
01-01 05:21:03.802  7258  7258 D RegisteredNfcFServicesCache: Service unchanged, not updating
01-01 05:21:03.802  7258  7258 D NfcService: Before mIsHceCapable
01-01 05:21:03.810  7258  7278 D NfcService: checking on firmware download
01-01 05:21:03.810  7258  7278 D NfcService: NFC is on. Doing normal stuff
01-01 05:21:03.811  7258  7278 I NfcService: Enabling NFC
01-01 05:21:03.811  7258  7278 D BrcmNfcJni: nfcManager_getChipVer: enter
01-01 05:21:03.811  7258  7278 D BrcmNfcJni: 0: nfcManager_getChipVer
01-01 05:21:03.816  7258  7278 D BrcmNfcJni: nfcManager_getNfcInitTimeout: enter
01-01 05:21:03.816  7258  7278 D BrcmNfcJni: NAME_NXP_DEFAULT_NFCEE_DISC_TIMEOUT not found
01-01 05:21:03.816  7258  7278 D BrcmNfcJni: NAME_NXP_DEFAULT_NFCEE_TIMEOUT not found
01-01 05:21:03.816  7258  7278 D BrcmNfcJni:  gNfcInitTimeout = 0: gdisc_timeout = 0 nfcManager_getNfcInitTimeout
01-01 05:21:03.816  7258  7278 I NfcService: Enabling NFC timeout90000
01-01 05:21:03.824  7258  7278 D BrcmNfcJni: nfcManager_doInitialize: enter; ver=NFCDROID-AOSP_M_00.01 nfa=NFA_PI_1.03.66+ NCI_VERSION=0x10
01-01 05:21:03.824  7258  7278 D BrcmNfcJni: nfcManager_doInitialize:  MW Version: NFC_NCIHALx_AR3C.7.4.0
01-01 05:21:03.824  7258  7278 D BrcmNfcJni: PowerSwitch::initialize: level=PS-FULL (1)
01-01 05:21:03.824  7258  7278 D NfcAdaptation: const CNfcParam *CNfcConfig::find(const char *) const found SCREEN_OFF_POWER_STATE=(0x1)
01-01 05:21:03.824  7258  7278 D BrcmNfcJni: PowerSwitch::initialize: desired screen-off state=1
01-01 05:21:03.824  7258  7278 D NfcAdaptation: NfcAdaptation::Initialize: enter
01-01 05:21:03.825  7258  7278 E NfcAdaptation: NfcAdaptation::Initialize: ver=NFCDROID-AOSP_M_00.01 nfa=NFA_PI_1.03.66+
01-01 05:21:03.825  7258  7278 D NfcAdaptation: const CNfcParam *CNfcConfig::find(const char *) const found PROTOCOL_TRACE_LEVEL=(0xFF)
01-01 05:21:03.825  7258  7278 D NfcAdaptation: NfcAdaptation::Initialize: NFA_EE_MAX_EE_SUPPORTED to use 2
01-01 05:21:03.825  7258  7278 D NfcAdaptation: const CNfcParam *CNfcConfig::find(const char *) const found APPL_TRACE_LEVEL=(0xFF)
01-01 05:21:03.825  7258  7278 D BrcmNfcJni: initializeGlobalAppLogLevel: level=5
01-01 05:21:03.825  7258  7278 D         : verify_stack_non_volatile_store
01-01 05:21:03.825  7258  7278 D NfcNciHal: crcChecksumVerifyIntegrity: filename=/data/nfc/nfaStorage.bin1
01-01 05:21:03.825  7258  7278 D NfcNciHal: crcChecksumVerifyIntegrity: filename=/data/nfc/nfaStorage.bin2
01-01 05:21:03.826  7258  7278 D NfcNciHal: crcChecksumVerifyIntegrity: filename=/data/nfc/nfaStorage.bin3
01-01 05:21:03.826  7258  7278 D NfcNciHal: crcChecksumVerifyIntegrity: filename=/data/nfc/nfaStorage.bin4
01-01 05:21:03.826  7258  7278 D NfcNciHal: crcChecksumVerifyIntegrity: filename=/data/nfc/nfaStorage.bin5
01-01 05:21:03.826  7258  7278 D         : delete_stack_non_volatile_store
01-01 05:21:03.828  7258  7281 D NfcAdaptation: NfcAdaptation::Thread: enter
01-01 05:21:03.829  7258  7282 I BrcmNfcNfa: NFC_TASK started.
01-01 05:21:03.829  7258  7281 D NfcAdaptation: NfcAdaptation::Thread: exit
01-01 05:21:03.830  7258  7278 D NfcAdaptation: NfcAdaptation::InitializeHalDeviceContext: enter
01-01 05:21:03.830  7258  7278 D NfcAdaptation: const CNfcParam *CNfcConfig::find(const char *) const found NCI_HAL_MODULE=nfc_nci.pn54x
01-01 05:21:03.830  7258  7278 E NfcAdaptation: NfcAdaptation::InitializeHalDeviceContext: fail hw_get_module nfc_nci.pn54x
01-01 05:21:03.830  7258  7278 D NfcAdaptation: NfcAdaptation::InitializeHalDeviceContext: exit
01-01 05:21:03.830  7258  7278 D NfcAdaptation: NfcAdaptation::Initialize: exit
01-01 05:21:03.830  7258  7278 I BrcmNfcNfa: nfa_dm_init ()
01-01 05:21:03.830  7258  7278 I BrcmNfcNfa: nfa_sys_register () id=1, enable_cplt_mask=0x0
01-01 05:21:03.830  7258  7278 I BrcmNfcNfa: nfa_sys_register () id=3, enable_cplt_mask=0x8
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_rw_init ()
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_sys_register () id=6, enable_cplt_mask=0x48
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_ce_init ()
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_sys_register () id=7, enable_cplt_mask=0xc8
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_ee_init ()
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_sys_register () id=2, enable_cplt_mask=0xcc
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_hci_init ()
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_hci_init() 10
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_hci_init() 2000
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: nfa_sys_register () id=8, enable_cplt_mask=0x1cc
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: LLCP - llcp_init ()
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: num_rx_buff = 21, rx_congest_start = 14, rx_congest_end = 10, max_num_ll_rx_buff = 6
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: max_num_tx_buff = 49, max_num_ll_tx_buff = 14
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: LLCP_RegisterServer (): SAP:0x1, link_type:0x2, ServiceName:<urn:nfc:sn:sdp>
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: LLCP_RegisterServer (): Registered SAP = 0x01
01-01 05:21:03.831  7258  7278 I BrcmNfcNfa: NFA_Enable ()
01-01 05:21:03.831  7258  7278 D NfcAdaptation: const CNfcParam *CNfcConfig::find(const char *) const found APPL_TRACE_LEVEL=(0xFF)
01-01 05:21:03.831  7258  7278 D BrcmNfcJni: initializeGlobalAppLogLevel: level=5
01-01 05:21:03.832  7258  7278 I BrcmNfcNfa: NFC_SetTraceLevel () new_level = 5
01-01 05:21:03.833  7258  7282 I BrcmNfcNfa: NFA got event 0x0100
01-01 05:21:03.833  7258  7282 I BrcmNfcNfa: nfa_dm_evt_hdlr event: NFA_DM_API_ENABLE_EVT (0x00)
01-01 05:21:03.833  7258  7282 I BrcmNfcNfa: nfa_dm_enable ()
01-01 05:21:03.833  7258  7282 I BrcmNfcNfa: NFC_Enable ()
01-01 05:21:03.833  7258  7282 I BrcmNfcNfa: nfc_set_state 0 (NONE)->1 (W4_HAL_OPEN)
01-01 05:21:03.834  7258  7282 D NfcAdaptation: NfcAdaptation::HalOpen
01-01 05:21:03.836  7258  7280 D NfcAdaptation: NfcAdaptation::NFCA_TASK: enter
01-01 05:21:03.836  7258  7280 I BrcmNfcNfa: GKI_run(): Start/Stop GKI_timer_update_registered!

Regards,

Gokulraj K.

0 件の賞賛
返信
1 返信

2,029件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

1. For your reference, the source code of the test.

nxpnfc_android_nougat/NfcFactoryTestApp.c at master · NXPNFCLinux/nxpnfc_android_nougat · GitHub 

Continuous RF ON is starting the Discovery loop for testing. PRBS is for PRBS test. (refer to UM10936 Chapter 12).

2. I think this is an Android developing issue.

etc/sample_nfcee_access.xml - platform/packages/apps/Nfc - Git at Google 

0 件の賞賛
返信