Where should RfReset be inserted within EMVCo CL1 loopback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where should RfReset be inserted within EMVCo CL1 loopback

Jump to solution
2,785 Views
deniscollis
Contributor V

Reference: EMVCo PCD Analogue Test Bench and Test Case Requirements Version 2.6b,

  1.  - page 74, Section 8.3. Preliminary Set-ups
  2.  - page 91, Section 8.8.1.3 TAB113.z00 Verifying the PCD Operating Field Resetting 

My contactless card reader recently failed test TAB113, as per reference b, above.  The test laboratory said they could not detect the RF-Reset within the loopback.   I challenged this as I believed this test case simply required manual invocation of a carrier reset by the operator. 

They rebuffed that they use "loopback" mode for ALL the Type Approval test cases, as per reference a, above.

On reviewing the NXP code, and some other alternates too, I see that there is only one 25ms RF reset, EmvcoRfReset(25) when exiting the loopback on an End_Of_Test_Analog (0x72) from the PICC.  Obviously this was not detected at all by the test bench. 

Where, then, should an additional RF Reset be inserted?

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
2,630 Views
deniscollis
Contributor V

Hi Kan,

It's a K81 + PN5180, but we're using a proprietary CL1 library.  The laboratory have subsequently informed us that the reader was performing within EMVCo specifications.  But the test bench timed out too soon (before the end of the final carrier reset in the polling procedure), and therefore was unable to detect the reset, which gave a false failure.  We've since reduced reset duration, and the test now passes. 

 

Thanks,

Denis

View solution in original post

0 Kudos
Reply
2 Replies
2,630 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Denis,

What is your contactless card reader? Which example project was running in the test TAB113? Was it NfcrdlibEx7_EMVCo_Polling? Please kindly clarify.

Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,631 Views
deniscollis
Contributor V

Hi Kan,

It's a K81 + PN5180, but we're using a proprietary CL1 library.  The laboratory have subsequently informed us that the reader was performing within EMVCo specifications.  But the test bench timed out too soon (before the end of the final carrier reset in the polling procedure), and therefore was unable to detect the reset, which gave a false failure.  We've since reduced reset duration, and the test now passes. 

 

Thanks,

Denis

0 Kudos
Reply