When will PN7150 support Android 11?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When will PN7150 support Android 11?

1,854件の閲覧回数
roman2004tw
Contributor I

Android 11 is planed to lunch at September 8, 2020.

When will NXP update the NXPNFCLinux to support  Android 11?

タグ(2)
0 件の賞賛
返信
1 返信

1,820件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, there is not more information for it so far. Sorry for the inconvenience may cause.

Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信