Very special antenna design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Very special antenna design

1,285 次查看
jof
Contributor I

My task is to design a antenna to read a mifare tag.

I try to describe the application:

Imagine a credit card shaped tag, but way smaller (25mm long, 11mm high, 3mm thick). This tag travels trough a tube with 15mm ID. This limits the turn of the card to the Z-Axis. So seen from a 0 degree point, the card can have any particular degree of turn from 0-359 degree.

At the postion of the reader, the card will be stopped, but cannot brought to a defined angle.

The reader antenna must be placed around the tube and has to be able to read the tag in any particular angle of Z.

Which antenna type/shape would be reccomended for this application? Maybe someone here knows about a similar application design.

Any help is appreciated

标记 (1)
0 项奖励
回复
2 回复数

1,187 次查看
jof
Contributor I

I'm using the CLRC663

0 项奖励
回复

1,187 次查看
jimmychan
NXP TechSupport
NXP TechSupport

which chip are you using?

0 项奖励
回复