Unable to add NxpNfcRdLib to static library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to add NxpNfcRdLib to static library

1,646 Views
jayesh_joshi
Contributor IV

Hi,

I am trying to create a static library that includes NxpNfcRdLib with it so that the application project doesn't have control over NxpNfcRdLib. I am successfully able to build a library project but when I add this lib to the application project and try to build an application project it is unable to add NxpNfcRdLib/intfs/phPlatform.h and all other header files from the folder. I have attached an image of the error. If I comment #inlcude <phPlatform.h> error shifts to the next line.

pastedImage_3.png

Labels (1)
0 Kudos
Reply
1 Reply

1,627 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Could you please try checking this post ?

How to create and use static library in MCUXpresso IDE 

Please let me know if that works for you !

Regards ,
Estephania

0 Kudos
Reply