USB Errors on ESD test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Errors on ESD test

3,528件の閲覧回数
jackchan
Contributor I

Hi,

I am using PN7462 for both smart card and NFC card reader.

I am suffering a problem with the ESD test.

USB communication will get lost in the ESD test but the device didn't aware of the situation.

The CPU is alive therefore watchdog is useless.

I am using like short D+/D- to simulate the ESD interference condition.

I discovered nothing abnormal from USB registers even the D+/D-  is shorted

The attached is the error counts from USB ISR.

To compare the snapshots, before and after D+/D- shorts, I got some questions:

#1. I got some NAK errors (isr_err[9]) even I did NOT enable the IntOnNak_AI/IntOnNak_AO/IntOnNak_CI/IntOnNak_CO bits of command/status register, before D+/D- get shorted. Where are they from and how?

#2. There is a sent stall error (isr_err[10]). I guess it is from the enumeration process but why? 

I did NOT find any abnormal during enumeration.

#3. After D+/D- get shorted, I tried several times and 2 samples attached.

One is reported truncated EOP (isr_err[8]) and one is reported bit stuff error (isr_err[13]). They are not always reported.

#4 What is the best way to detect USB interface errors. Original I  think it can be detected by SOF and NAK of interrupt endpoint. Both of them could be beacons between the USB host and the device. However, I can get SOF and NAK ISRs when the D+/D- get shorted, but I think the communication between the USB host and the device actually gets lost since card insertion even is bot work anymore.

Are there any registers that need to be set to properly detect SOF/NAK behavior correctly?

Jack

0 件の賞賛
返信
1 返信

3,454件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

The PNEV7462 board is ok with USB certificate, please kindly refer to the following for details.

pastedImage_1.png

I think it should be a hardware design issue, please refer to the ref board schematics (UM10883 )and check if there is  any difference . 

BTW, what is the ESD voltage level performed on PN7462?

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信