UCODE G2iM+ current consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UCODE G2iM+ current consumption

1,785 Views
info25
Contributor I

Hi,

We're designing a new product using the UCODE G2iM+ (SL3S1013), and there seems to be contradictive information regarding the minimum current consumption.

Table 36 in the datasheet (SL3S1003_1013, Rev. 3.8 — 5 February 2019) says 14 uA.

Section 3.2 in the application note (AN10940, Rev. 1.3 — 13 May 2014) says 7 uA.

What is the correct value?

Thanks in advance.

0 Kudos
Reply
2 Replies

1,724 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi  , 

I believe there is a confusion here,you are comparing G2iL+ (7uA) values with G2iM+ (14uA) – the issue here is not necessarily the max. values.

  • Section 3.2 in the application note (AN10940, Rev. 1.3 — 13 May 2014) the diagram is based on G2iL+
  • Datasheet (SL3S1003_1013) – is the datasheet of the G2iM & G2iM+

Have a great day !

BR

Jonathan

0 Kudos
Reply

1,724 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

I have modified my answer due to some erros and got  of data confirmation please check it above.

Have a great day !

BR

Jonathan

0 Kudos
Reply