Trying to use CLRC663 to read and write UID and data over desfire

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trying to use CLRC663 to read and write UID and data over desfire

5,648 次查看
mohamed_elsabagh
Contributor I

Hello, We are working on a project where we are using nrf52 MCU as host controller with CLRC663 reader. Until now we have been able to get UID from mifare classic tags, and read/write on different sectors/blocks. Now we need to start supporting Desfire EV2/3, but I can't find any usable codes or low level steps to:

1. Get the UID from a tag

2. Read/Write Customer user data to the tag.

 

Can anyone please help with this, thanks and BR.

标记 (2)
0 项奖励
回复
6 回复数

4,978 次查看
Akhil_Puranik
Contributor II

Hi @mohamed_elsabagh  I am now trying to interface CLRC663 with nRF52832 to read UID and card data.
Can you please share the references you have used for doing it?
In addition to that, if you can share the Library files it will be of great help to me.

标记 (2)
0 项奖励
回复

5,621 次查看
JHinson
Contributor I

Hi Fang Fang

Mohammed is a developer inthe eLocker team, we have already signed the NDA but I cannot locate the SW375617 file on our account, I think we need a higher access level to be able to download this file, please can you allow us access?


Thanks

 

Jacob

0 项奖励
回复

5,607 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

In case you are not able to find it, please request it in My Access section -> Access Rights and provide a description why you need it ; here also provide NDA number to speed things up for the reviewer. Finally  send request.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复

5,638 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The related code is NDA. So you need an NDA to gain access to that documentation. If you has  NDA. Please refer to the attachment how to find the document on Docstore. 

Have  a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复

5,632 次查看
mohamed_elsabagh
Contributor I

So In order just to read UID of a desfire EV2/EV3 using nxp chip CLRC663 this needs NDA?

 

And to start writing and reading custom application data on desfire, I need this as well? so how can I get an NDA in this case?

0 项奖励
回复

5,633 次查看
fangfang
NXP TechSupport
NXP TechSupport
 
0 项奖励
回复