To driver pn532 with libnfc-nci

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To driver pn532 with libnfc-nci

ソリューションへジャンプ
3,222件の閲覧回数
rodger_an
Contributor I

Hello, I have a question. Can I use libnfc-nci to drive pn532? Do we have any instructions if it can be drived. I am looking forward to your feedback. Thank you!

0 件の賞賛
返信
1 解決策
3,216件の閲覧回数
AlexanderB
NXP Employee
NXP Employee

Hi @rodger_an ,

theoratically yes. But you would have to implement some kind of translator as man-in-the-middle as the PN532 is not native NCI.

If you want to drive a NFC controller with the libnfc-nci I recommend to have a look at the PN7160. That should be kinda plug&play and exactly for that purpose.

Best regards,
Alexander

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,217件の閲覧回数
AlexanderB
NXP Employee
NXP Employee

Hi @rodger_an ,

theoratically yes. But you would have to implement some kind of translator as man-in-the-middle as the PN532 is not native NCI.

If you want to drive a NFC controller with the libnfc-nci I recommend to have a look at the PN7160. That should be kinda plug&play and exactly for that purpose.

Best regards,
Alexander

0 件の賞賛
返信
3,185件の閲覧回数
rodger_an
Contributor I

Thanks for your reply. I will have a look into it.

0 件の賞賛
返信