Tamper detection using NXP Cockpit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tamper detection using NXP Cockpit

1,795 次查看
GabCelestica
Contributor I

I'm using the CLEV6630A V2.0 with a tamper detection tag (ISO 15693) with the ST25TV chip but I am not able to check the tamper status using the NXP cockpit. Any idea if this can be done and how?

Thank you very much!

0 项奖励
回复
2 回复数

1,763 次查看
GabCelestica
Contributor I

Good Afternoon,

Thank you very much for your response. I would like to read a configuration block with the command A0h and read the block 5h.

The frame I would like to send is 22A0028441AD21002302E005

Being:

22 : Flags

A0 : Command

02 : Mfg Code

8441AD21002302E0 : UID

05 : Pointer

Is there a possibility of using the NXP Cockpit to send a personalized frame?

Thank you very much for your help

0 项奖励
回复

1,782 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

You will need to verify if your tag has some register with the status and try to read the register form the reader. You will need to know the commands, the register and that everything is according to the spec of the ISO 15693.

 

regards,

Estephania

 

 

0 项奖励
回复