Supporting ISO15693 using PN7120 Kit.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supporting ISO15693 using PN7120 Kit.

1,769 Views
sangdolee
Contributor I

Hi,

We got PN7120 Kit and port libnfc-nci to Raspberry-pi.

And, we have to read data from ISO15693 card.

But, I am not sure libnfc-nic can support ISO15693.

Demoapp seems not to have ISO15693 procedure. Am I right?

I don't know about NFC. I just want to read 15693 card.

What is best idea?

Studying NFC? :smileysad:

BR

Paul

0 Kudos
Reply
1 Reply

1,471 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Paul,

Yes, libnfc-nic can support ISO15693.You may refer to NFC_Reader_Library\NxpNfcRdLib\comps\phpalSli15693 for details. and LPC based demo can be downloaded from http://cache.nxp.com/documents/software/SW3241.zip . Please kindly refer to the following for more details.

pastedImage_2.png


Wish it helps.

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply