Straight forward 14443B protocol like a rs232 port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Straight forward 14443B protocol like a rs232 port

1,358 Views
hanktan
Contributor II

I'm trying to use a pair of rc531 boards to bridge between the card and reader, and analyze character streams passing between them. There is an app called NFC SPY can easily control 2 android phones to bridge between the card and the reader. I want to know what (cos) commands to set the 531 to behave just output any streams converted from NFC 14443B physical signal without to to identify any card number or Device ID or any poking into the stream. Attached is the NFC SPY bridge data stream result 

0 Kudos
Reply
1 Reply

1,231 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Hank,

There is no such kind of command for your requirement, maybe you have to built a costom application to implement this function.

Have a great day!

Kan

0 Kudos
Reply