Reset EAS using Flutter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset EAS using Flutter

ソリューションへジャンプ
2,103件の閲覧回数
fadzlihakim
Contributor I

Hi. I'm developing Flutter using plugin flutter_nfc_kit that support transceive().

Currrently facing a problem to reset EAS.

NFC: NXP ICODE SLIX

 

 

Uint8List command = Uint8List(10);

command[0] = 0xA3; // Reset EAS

command[1] = 0x04; 

command[2...9] = UID

await FlutterNfcKit.transceive(command);

 

 

Response from transceive: [1, 15]. After ehecking with alarm EAS still activated.

 

If someone can help me to solve the problem it would be great.

Thank you.

0 件の賞賛
返信
1 解決策
2,062件の閲覧回数
fadzlihakim
Contributor I

HI.

I just found solution for the problem.

Uint8List command = Uint8List(0);
command[0] = 0x22; // Flag Address
command[1] = 0xA3; // Reset EAS
command[2] = 0x04; // IC manufacture code
command[3...10] = UID; 
await FlutterNfcKit.transceive(command);

 I able to send command to read multiple blocks and to write AFI and tags is not password protected.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,063件の閲覧回数
fadzlihakim
Contributor I

HI.

I just found solution for the problem.

Uint8List command = Uint8List(0);
command[0] = 0x22; // Flag Address
command[1] = 0xA3; // Reset EAS
command[2] = 0x04; // IC manufacture code
command[3...10] = UID; 
await FlutterNfcKit.transceive(command);

 I able to send command to read multiple blocks and to write AFI and tags is not password protected.

0 件の賞賛
返信
2,071件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello,
Thank you for using our products.
I'm very sorry but, we can't be sure on what could be causing this issue. Since we don't have any knowledge of Flutter. We do have an Android app that shows the tag UID but, is only for testing purposes. My recommendation would be to please take a look at our ICODE SLIX documentation section 9.4.3.
As mentioned in the command section (9.4.3.8) Is there any chance that the tag is password-protected?
Are you able to correctly send any other command to the Tag? i.e. Reader Single Block.

Best Regards,
Fabian
0 件の賞賛
返信