Reader for ISO14443

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reader for ISO14443

3,124 Views
johnmax
Contributor I

Is there any >1W reader available for ISO14443?

0 Kudos
Reply
2 Replies

2,738 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello jhon max:

You may have a look to the PN5180 NFC frontend. This is a high-power NFC IC with the RF driver supply voltage from 2.7 V to 5.5 V and max driver current of 250 mA.

Regards!

Jorge Gonzalez

0 Kudos
Reply

2,738 Views
rfidtag
Contributor II

Hi John,

As I far know syncotek.com  produce 2W HF reader ISO 15693 maybe  they are able to offer also ISO14443.

Regards,

Libor

0 Kudos
Reply