RFID - long read range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RFID - long read range

2,719 Views
jakub_
Contributor I

Hi,

our new design requires RFID identification of tool used in home appliance. Required reading distance is about 35 cm. We consider 13.56 MHz as best fitting our application, but consider also LF technology. Can you recommend any solutions / ICs suitable for this application?

Regards,

Jakub

0 Kudos
Reply
2 Replies

2,437 Views
jakub_
Contributor I

Thank you, but this is what we've already known - we can build this with Hitag family or with ISO 15693 chips @ 13.56 MHz. I hoped there are somewhere "hidden" reference designs or guidelines regarding read range vs antenna size and power or power boosting circuits, if necessary, as TI provides on their e2e forum:

TRF7960 antenna size - NFC/RFID Forum - NFC/RFID - TI E2E Community

Regarding Power amplifier for TRF7960EVM - NFC/RFID Forum - NFC/RFID - TI E2E Community 

Regards,

Jakub

0 Kudos
Reply

2,437 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the following link for more information about the RFID operating Distances:

RFID Technology|NXP 

 

Have a great day!

 

Regards,

Ivan.

0 Kudos
Reply