RFID - Read and Write

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RFID - Read and Write

6,100件の閲覧回数
eliezeroc
Contributor III

Hello everyone;

I'm trying to develop a code to read and write in 1K tags but I'm not getting.

My project will make control of vehicles entering a parking lot.

Can anyone ajusdar me?

Thank you.

5 返答(返信)

4,947件の閲覧回数
nguyenhai
Contributor I

Hi Jorge_Gonzalez Employee

I want to more some information about RFID reader.

I'm designing a full solution for warehouse management system, and knowing that NXP RFID solution is good choice.

0 件の賞賛
返信

4,946件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eliezer Oliveira:

Thank you for using our community.

Please let us know more details about your issue:

Which NFC Reader IC are you using?

What type of tags you need to read?

Are you working from an existing software framework or code example?

What is the erratic behavior you see?

With this information we can provide better feedback.

Regards!

Jorge Gonzalez

4,947件の閲覧回数
eliezeroc
Contributor III

Hello Jorge Gonzalez, thank you for your attention.

1 - I am using MFRC522;

2 - I need to read Mifire tags 1K;

3 - I'm working with sample code.

4 - The code compiles without problem, but I can not read the tag, does nothing.

Already come some time working on it.

I'm using to communicate with the RFID module, the SPI0 PT60 micro controller;

If you need more information I have great pleasure in passing, and again thank you for your support.

4,947件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eliezer:

Thank you for responding to my questions.

The MFRC522 initialization and the protocol used to communicate to MIFARE cards is kind of complex. That is why NXP provides the NFC Reader library. Unfortunately the library is currently available for some LPCXpresso boards such as LPC1769 and LPC11U68. Porting to a different MCU platform or using a third party sample code or stack is out of our support scope.

Sorry for the inconvenience.

Regards!

Jorge Gonzalez

0 件の賞賛
返信

4,947件の閲覧回数
eliezeroc
Contributor III

Hello Jorge Gonzalez.

Hand me the information so I can develop my project.

If possible, give me everything you can as:

microcontroller;

libraries;

Links to download;

manuals;

Examples.

I am willing to make changes to my project so I have success.

Thanks in advance.