RC522,how can i send data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RC522,how can i send data?

2,012件の閲覧回数
suhaihui
Contributor I

there is how i send data.

1.reset tx rx point.

1.write data to fifo

2.set startsend to 1.

but i measure tx1 and tx2 wave, i can't find the modulated wave.(I want to find mifare card, so ASK=100%).

there only have 13.56MHz wave i can found. 

0 件の賞賛
返信
1 返信

1,821件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Su Haihui,

The attachment is a script for RC522 reading Mifare card, please refer to it for details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------