Question about PN5180 datasheet, RANDOM_UID_ENABLE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about PN5180 datasheet, RANDOM_UID_ENABLE

跳至解决方案
2,083 次查看
OilCastle
Contributor III

Hello, I have some questions about PN5180 datasheets.

 

In section 11.5.2 EEPROM (Table 51.), address [0x51] and [0x58] have same descriptions.

I'm little confused. Should I use both or what? or is it some typo?

 

jun-younglee_0-1616553055220.pngjun-younglee_0-1616553055220.png

 

And what's the difference data sheet suffix "_C3_C4" and "-C1-C2"

Is "PN5180A0XX-C1-C2.pdf" document just older version of "PN5180A0XX_C3_C4.pdf" ?

 

FYI, I attach some part of EEPROM address table from "PN5180A0XX-C1-C2.pdf". 

jun-younglee_1-1616553560235.pngjun-younglee_1-1616553560235.png

As you can see, it's from first image. 

 

Thanks, and have a good day.

 

0 项奖励
回复
1 解答
2,067 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 The 0x51 is the value to activate the RandomID and the 0x58 stores the UID03.

And the difference of the C1/C2 and C3 version is Firmware version. Please refer to the datasheet for the detail information.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,068 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 The 0x51 is the value to activate the RandomID and the 0x58 stores the UID03.

And the difference of the C1/C2 and C3 version is Firmware version. Please refer to the datasheet for the detail information.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复