Program/flash PN7462 without MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program/flash PN7462 without MCUXpresso IDE

ソリューションへジャンプ
2,581件の閲覧回数
lucasj
Contributor II

Hello everyone,

I have developed a firmware for the PN7462 microcontroller. I have been using MCUXpresso IDE with LPC-Link 2 to program the firmware. However, this method would be tedious for production porposes. Is there a simpler way to flash the binary without using MCUXpresso IDE? A command line tool would be nice, since it allows us to automate the process using test Jigs.

I want something like the ST's STM32CubeProgrammer, which has both graphical and command line interfaces just to manage ST microcontrollers memory through a ST-Link device.

0 件の賞賛
返信
1 解決策
2,567件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Lucas:

 

You can use jlink or flash magic.

https://www.flashmagictool.com/

 

Regards

Daniel

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,568件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Lucas:

 

You can use jlink or flash magic.

https://www.flashmagictool.com/

 

Regards

Daniel

 

 

 

 

0 件の賞賛
返信