Power consumption on RFID chip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Power consumption on RFID chip

675 次查看
hengma
Contributor II

Hi,

 

I would like to measure the current consumption ITVDD of RFID chips such as CLRC663 or PN5180.  The proposed idea is that we can turn on the RF and measure the output voltage of the current sense amplifier. Is the solution reasonable?

 

Thanks,

Heng

标记 (1)
0 项奖励
回复
3 回复数

657 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @hengma

Hope you are doing well.

ITVDD can be measured between the source and TVDD pin. If you are using the OM26630FDK Dev Kit or the OM25180FDK Dev Kit, you can use jumper J300 to measure ITVDD.

Regards,
Eduardo.

0 项奖励
回复

645 次查看
hengma
Contributor II

Hi Eduardo,

 

Thanks for your response, however, in real user cases, we can not use an amp meter to measure the current consumption. The solution in the AN11022 is for the engineering development process. We would like to have a more user-friendly way to measure the current consumption of the CLRC633. Can we use a current sensing amplifier such as INA181 and measure the current consumption when RF is on? m

 

Thanks,

Heng

0 项奖励
回复

626 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

There is no specific tool or device I could recommend. Which method to use is up the customers based on their needs, and considering CLRC663/PN5180 characteristics and parameters described in their corresponding Data Sheet.

Regards,
Eduardo.

0 项奖励
回复