Porting CLRC663 on Android 7.1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting CLRC663 on Android 7.1.2

2,861 Views
engineer_bsp01
Contributor III

Hi,

We are working on Quectel SC20 module runs on android 7.1.2 .NXP CLRC663 reader is used for NFC communication.

we put drivers of CLRC663 in the path kernel/drivers/nfc.

What else has to be done in the source code of android 7.1.2 for porting CLRC663?

Regards,

RICHU C J

4 Replies

2,517 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi RICHU,

    For NFC application on android, PN7150 & PN7120 are recommended for customer.

PN7150: PN7150 | High performance NFC controller for smart devices | NXP 

PN7120: PN7120 |NFC controller with flexible host interface for Home appliances | NXP 

    From descripitons and documents on weblink, you will find these 2 NFC readers are Very suitable for applications with operating systems.

    CLRC663 is suitable for application without OS or FreeRTOS or  Processors + linux application, we don't have solutions on  CLRC663 working on Android platform.

Hope above information can help you!

Have a nice day!

Best Regards,

Weidong

1,862 Views
thieuqp
Contributor II

Dear Mr!

Do you have any document to guide porting PN71xx to Android, pls help me share.

Thanks

0 Kudos
Reply

2,517 Views
engineer_bsp01
Contributor III

Hi Weidong,

Thanks for your reply

Best Regards,

Richu

0 Kudos
Reply

2,517 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Welcome!

0 Kudos
Reply