PNEV5180B with external MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PNEV5180B with external MCU

Jump to solution
1,829 Views
bryan3
Contributor I

I'm starting to use the PNEV5180B dev kit and would like to interface it with an external MCU. Do I need to/how can I bypass the connections of the PN5180 with the LPC1769 and just jump the connections to my external board?

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,741 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bryan,

Please kindly refer to "5.2 Connecting the FRDM-K82F to the PNEV5180B" in the following links:

https://www.nxp.com/docs/en/application-note/AN11908.pdf 

The steps can also be applied for any other external MCU.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,742 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bryan,

Please kindly refer to "5.2 Connecting the FRDM-K82F to the PNEV5180B" in the following links:

https://www.nxp.com/docs/en/application-note/AN11908.pdf 

The steps can also be applied for any other external MCU.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply