PN7642 Mass Storage Device Activation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7642 Mass Storage Device Activation

ソリューションへジャンプ
2,601件の閲覧回数
MLang
Contributor II

I am attempting to flash the firmware required for the Cockpit application on to a PNEV7642A development board. I am unable to get the USB port to enumerate as a mass storage device on my PC.

I think that I have the host interface correctly configured for USB using switches 5, 6, and 7. I have held down and released various combinations of the the VEN and DWL_REQ buttons without success.

The unit is powered from a 7.5V supply on J9.

I've read through through the various applications guides and these are main things that appear to be required.

What am I doing wrong? Thanks. 

ラベル(2)
0 件の賞賛
返信
1 解決策
2,548件の閲覧回数
MLang
Contributor II

I resolved this myself.

If the PNEV7642A is not connected to the LPC55S16 dev board, the AD_NFC_HOSTSEL2 line is unterminated and allowed to float. This can prevent the USB interface from being enabled. Terminating this line to +3.3V properly enabled the USB interface allowing proper mass storage device operation.

This should probably be included as a note in the quick start guide.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,592件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,
My name is Fabian, I'm happy to help you with your case.
Thank you for your interest in our products. Would you mind sending us a photo of your setup just to scratch any possible issues?

Best Regards,
Fabian
0 件の賞賛
返信
2,549件の閲覧回数
MLang
Contributor II

I resolved this myself.

If the PNEV7642A is not connected to the LPC55S16 dev board, the AD_NFC_HOSTSEL2 line is unterminated and allowed to float. This can prevent the USB interface from being enabled. Terminating this line to +3.3V properly enabled the USB interface allowing proper mass storage device operation.

This should probably be included as a note in the quick start guide.

0 件の賞賛
返信