PN7642 Antenna Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7642 Antenna Design

1,613 Views
MPEngineering
Contributor I

Hey there,

i´m currently designing an custom PCB with PN7642 and i wanted to ask, if somebody has experience with the minimum size of a custom antenna.

The PCB is quite small. The problem i see is, that if underneath the antenna is a solid GND or VCC plane, much power dissipates into it, right? In that case the size would be about 37 x 12 mm.

The size with plane free area for the antenna could only be 17,25 x 9,5 mm.

Could this be enough?

 

Best regards

Oliver

0 Kudos
Reply
3 Replies

1,594 Views
MPEngineering
Contributor I

Hey KaiLi,

thanks for replying. I know this Guide, but there is nothing about the Shape for the Antenna itself, only recommendations for routing the BGA.

I´ve read in the "PN7160 antenna design and matching guide", that the smaller the antenna, the smaller the reading distance.

But what is meant with small? Or is it try and error princip?

 

 

0 Kudos
Reply

1,590 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MPEngineering 

"Small" means small in size. Please refer to Figure 2 in Chapter 2.1 of  PN76 family antenna design guide

The shape and size of the antenna depend on your application requirements. You can also use the NXP recommended design. For the PN7642, the antenna can be square with a size of 45*45mm.

0 Kudos
Reply

1,598 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @MPEngineering 

It's recommanded that you try online NFC Antenna Tool NFC - NXP Community to design antenna according to your application Scenario.

For pcb layout, please check PN76 family antenna design guide, especially 3.3 section.

0 Kudos
Reply