PN7462 for Mac IDE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 for Mac IDE?

5,924 Views
mariob
Contributor III

Hi right now there is only a PN7462(com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-155) plugin for the Windows version of LPCXpresso. Is there a possibility to get a plugin for the Mac version as well?

Best Regards Mario

Labels (2)
0 Kudos
Reply
9 Replies

5,586 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

5,586 Views
mariob
Contributor III

Hi jimmychan,

thank you for your support.

I know where to download the MAC version of the IDE. That is not the point.

My LPCXpresso is running and works fine. etc. with an LPCXpresso1769 board.

But for the PN7264 you need a plugin for the IDE. 

The plugin you can download here:

PN7462 | All-in-one NFC Cortex-M0 MCU 160kB Flash|NXP 

is only for the Windows version.

Best Regards Mario

0 Kudos
Reply

5,586 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mario,

As you posted in https://community.nxp.com/thread/437646#comment-846237 , you have already found a solution for this, was it just for VM(Mac) under windows? Is the problem still there with a real Mac machine? What is the Mac version on your side? Please kindly help to clarify.

Thanks for your patience!

-Kan

0 Kudos
Reply

5,586 Views
mariob
Contributor III

Hi Kan,

the solution i have found was for a Virtual Windows machine on my MAC(VM Ware Fusion).

My OS Version ist: macOS Sierra Version 10.12.1

LPCXpresso Version: 8.2.2

Best Regards 

Mario

0 Kudos
Reply

5,586 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mario,

Please use the PN7462 plugin from https://www.nxp.com/webapp/Download?colCode=SW3683&location=null&Parent_nodeId=145936388269572902024... for LPCXpresso MAC version, but it is required to use LPCXpresso v8.0.0.

Please install this version, activate it and add plugin, this should work.

Please kindly let me know if the problem is still there.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,586 Views
mariob
Contributor III

Hi Kan,

i installed version 8.0.0 of LPCXpresso. I also downloaded the file you told me.

This is the sam file I have already downloaded, right? It is an *.exe witch I i have to run on a

Windows machine to get extracted. 

After installing the plugin in LPCXpresso 8.0.0 on my Mac I ended with the following error:

Error Message.png 

I tried to fix this by copying the files for the Windowsmachine into the corresponding folder.

Here is the Result:

Error.png

Did I make a mistake somewhere?

Best Regards

Mario

0 Kudos
Reply

5,586 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mario,

From the above line you should have an exe file and executing it will get a zip file like the following:

pastedImage_1.png

but would you please specify how you install this patch? just extract it or install it by LPCXpresso->Help->Install New Software like below:

pastedImage_2.png

Please kindly help to clarify. Thanks for your patience!

B.R

Kan

0 Kudos
Reply

5,586 Views
mariob
Contributor III

Hi Kan,

of corse I installed the file, as you can see here:

plugin.png

Hope that helps

Best Regards 

Mario

0 Kudos
Reply

5,586 Views
jimmychan
NXP TechSupport
NXP TechSupport

let me check this with the expert

0 Kudos
Reply